News

10 July 26

Circuit symbols explained: a UK guide

A circuit symbol is a standardised shorthand for a component. In the UK, schools, exam boards and industry all use the same standard — BS EN 60617, the British version of the international...Read the full story

10 July 26

Rapid supports Engineering Student Awards at Colchester Institute

Rapid Electronics was proud to support the recent Engineering Student Awards Event at Colchester Institute through the donation of Rapid branded multimeters for award-winning students. Combining p...Read the full story

09 July 26

Understanding K-type thermocouples

The K-type is the general-purpose workhorse of temperature measurement: a chromel–alumel thermocouple covering roughly −200°C to +1260°C, cheap to make, tough enough for industrial use and supported...Read the full story

09 July 26

Terminal blocks: types, specs & how to choose

The short answer A terminal block is chosen on five parameters: pitch, current and voltage rating, conductor cross-section, pole count, and connection method. Pitch is the unforgiving one — i...Read the full story

08 July 26

MPU6050 alternatives: what to use now the chip is EOL

The MPU6050 motion sensor module has been the default six-axis IMU for a decade of Arduino, Raspberry Pi and micro:bit projects — a three-axis gyroscope and three-axis accelerometer on one chip, tal...Read the full story

07 July 26

T568A and T568B colour codes for ethernet cable wiring

Ethernet cables are wired to one of two colour standards: T568A or T568B. Both use the same four twisted pairs - orange, green, blue and brown - and differ only in one detail: the orange and green p...Read the full story

07 July 26

Choosing the right electronic enclosure

The short answer Choose an enclosure by working from the environment inwards, not from the PCB outwards. Fix the installation environment first — that sets your IP and IK ratings, which set y...Read the full story

06 July 26

Ohm's law explained: how voltage, current and resistance relate

Ohm's law states that the current through a conductor is proportional to the voltage across it: V = I × R, where V is voltage in volts, I is current in amps and R is resistance in ohms. Rearrange it...Read the full story

06 July 26

NE555P alternatives and equivalents: what to use instead

The Texas Instruments NE555P is the standard bipolar 555 timer in a DIP-8 package, probably the most recognisable IC part number in electronics, and still in volume production more than fifty years ...Read the full story

03 July 26

Temperature conversion: Celsius, Fahrenheit and Kelvin explained

Converting between temperature scales comes down to two formulas: multiply Celsius by 1.8 and add 32 to get Fahrenheit, and add 273.15 to Celsius to get Kelvin. That covers the arithmetic, but in el...Read the full story

03 July 26

Wire gauge conversion chart: AWG to MM2 explained

Wire gauge conversion trips people up because three sizing systems are in everyday use in UK workshops: AWG (American Wire Gauge) on imported components and US-authored schematics, metric mm² on Europ...Read the full story

18 June 26

Pass/fail vs. downloadable PAT testers: comparing ROI & speed efficiency

Choosing the right Portable Appliance Testing (PAT) equipment is one of those decisions that looks simple on the surface but can quietly cost or save your business thousands of pounds over time....Read the full story

17 June 26

Arduino UNO Q in industry: accessible edge AI, built for the real world

Industrial automation is changing faster than most budgets can keep up with. Businesses need intelligent systems, AI-driven inspection, predictive maintenance, smart factory integ...Read the full story

17 June 26

Toroidal vs EI core transformers: space, noise and efficiency compared

Choosing the right transformer is often a balance between performance, cost and physical constraints. For engineers designing audio equipment, semiconductor test systems, medical devices or in...Read the full story

12 June 26

Common test & measurement challenges and the equipment that solves them

Modern electronic systems are becoming faster, more complex and more integrated than ever before. As a result, engineers face a growing range of test and measurement challenges...Read the full story

11 June 26

What to look for in a test & measurement distributor

Choosing the right test and measurement equipment is an important decision, but choosing the right distributor can be just as critical. Whether ...Read the full story

11 June 26

Eliminating upgrade risks at Dalhousie Castle

How Chauvin Arnoux UK's PEL113 power loggers provided the critical data needed to greenlight an 86.5 kW infrastructure modernisation with zero operational downtime. ...Read the full story

08 June 26

Common applications of chassis mount transformers in industry

Chassis mount transformers are a core component in many industrial electrical systems, providing reliable voltage conversion, isolation and power distribution. Designed for secure mounting within encl...Read the full story

08 June 26

How to choose the right power supply unit (PSU) for industrial applications

Selecting the right power supply unit (PSU) is critical to ensuring the reliability, efficiency and safety of industrial systems. Whether you’re powering control panels, automation equipment or embedd...Read the full story

08 June 26

Using heavy duty enclosures in harsh environments

Heavy duty enclosures are designed to protect critical electrical and electronic components in some of the most challenging operating conditions. From offshore installations to dusty manufacturing pla...Read the full story

08 June 26

PCB terminal block selection guide for engineers

Selecting the right PCB mount terminal block is critical for ensuring reliable electrical connections, long-term performance and ease of maintenance. Whether used in industrial control systems, power ...Read the full story


Trustpilot