An uninterruptible power supply does a more modest job than its name suggests, and understanding that is the key to buying the right one. A typical UPS exists to bridge the gap between the mains failing and equipment shutting down safely — minutes of battery, not hours — while also smoothing over the sags, spikes and flickers that outnumber real outages a hundred to one. Sized and specified well, it turns a power cut from data loss and a ruined 3D print into a non-event; specified on the headline number alone, it disappoints on the first outage.
This guide covers the three UPS topologies and what each actually protects against, the VA-versus-watts trap in the ratings, how to size for load and runtime honestly, the waveform detail that matters for modern equipment, and the battery realities that decide whether the UPS works on the day it's finally needed.
What are the three types of UPS?
| Topology |
How it works |
Suits |
| Standby (offline) | Passes mains straight through; switches to inverter on failure, with a transfer gap of a few milliseconds | PCs, home network gear, non-critical kit that tolerates the blink |
| Line-interactive | Adds automatic voltage regulation, correcting sags and swells without touching the battery | Servers, NAS, lab and workshop equipment on imperfect mains — the sensible mid-tier default |
| Online (double-conversion) | Rebuilds the output continuously from the inverter; zero transfer time, complete isolation from mains disturbance | Critical systems, sensitive instruments, harsh industrial supplies |
The differences matter because most power problems aren't outages. Brownouts, sags from heavy machinery starting nearby, and momentary flickers are far more frequent, and a standby UPS answers them only by dropping to battery each time — cycling the battery towards early death. Line-interactive regulation absorbs that daily abuse electronically, which is why it owns the middle of the market; double-conversion is the answer when the equipment can't tolerate even a millisecond gap, or the incoming supply is genuinely hostile.
What do the VA and watt ratings mean?
Every UPS carries two capacity numbers, and the marketing leads with the bigger one. Volt-amps (VA) is apparent power; watts is the real power the UPS can actually deliver, and the ratio between them — the power factor — typically runs from about 0.6 on budget units to 0.9 or better on quality kit. A "1000 VA" UPS with a 0.6 power factor is a 600 W device, and connecting 800 W of equipment to it overloads it despite the sums appearing to fit. The rule: size against the watt rating, add 20–30% headroom for inrush and future growth, and treat the VA figure as advertising.
Runtime follows its own nonlinear arithmetic: batteries deliver disproportionately more minutes at light load, so halving the connected load usually far more than doubles the runtime. Manufacturers publish runtime-versus-load charts for exactly this reason — read the chart at your real load rather than trusting the headline "up to" figure, which describes a nearly empty UPS.
What should — and shouldn't — plug into a UPS?
On the battery-backed sockets: the equipment whose ungraceful death costs something — the computer and its storage, the network switch and router that everything else needs, the controller mid-process, the instrument mid-measurement, the 3D printer mid-print. On the surge-only sockets most UPSs also provide: monitors, peripherals, things that can die and return without consequence. And on the wall, never the UPS: laser printers, whose fuser draws kilowatt pulses that overload a UPS instantly; heaters and motors for the same reason. A UPS also isn't a substitute for dedicated surge protection at the distribution level — it includes suppression, but its job is continuity, not absorbing lightning.
The detail that completes the system is communication: a USB or network link from UPS to computer, so that when the battery runs low during a long outage, the machine saves and shuts itself down unattended. A UPS without the shutdown link protects against short cuts and merely postpones long ones.
Does the output waveform matter?
Increasingly, yes. Budget UPSs produce a stepped approximation of a sine wave on battery, which older power supplies accepted happily. Modern equipment with active power factor correction — which includes most current PC and server supplies — can misbehave on simulated sine: shutting down, clicking in and out, or stressing the PSU precisely at the moment the UPS is supposed to be saving it. If the connected kit is modern and mattered enough to protect, specify pure sine wave output; the premium has shrunk to the point where it's cheap insurance against a compatibility failure discovered mid-outage.
What kills UPS batteries, and when do they need replacing?
The standard sealed lead-acid battery inside a UPS is a consumable with a service life of roughly three to five years — and heat is its enemy: life halves for something like every 8°C above room temperature, which is why a UPS in a warm rack or a sunlit corner ages its battery at double speed. The failure mode is quiet: the UPS sits green and content until an outage reveals a battery that holds seconds instead of minutes. The defences are routine rather than clever — run the self-test periodically, replace batteries on schedule rather than on failure, favour models with user-replaceable packs so the swap is a cartridge change rather than a new UPS, and give the unit ventilation. Lithium-based UPSs stretch the replacement interval considerably at a higher purchase price — an increasingly sensible trade in installations where access is awkward. A battery tester settles arguments about marginal packs, and the wider batteries and chargers range covers replacements.
What about DC systems and panels?
The same continuity problem exists inside control panels and embedded systems, where the loads are 12 or 24 V DC and a mains UPS is the wrong shape for the job. DIN-rail DC UPS and buffer modules sit between an open-frame or DIN-rail PSU and the load, holding the DC bus up through interruptions — the panel-builder's equivalent of everything above, protecting PLCs and controllers through the dips that would otherwise reboot a production cell. For bench and product work, the broader power supplies range covers the supply side that the UPS exists to back up.
Featured power protection
Frequently asked questions
How long will a UPS run my equipment?
Typically minutes at meaningful load — a UPS is designed to bridge to a safe shutdown or a generator, not to power through an outage. Runtime rises steeply as load falls, so check the manufacturer's runtime chart at your actual wattage rather than the headline figure.
What's the difference between VA and watts on a UPS?
VA is apparent power; watts is what the UPS can really deliver, related by its power factor — often 0.6 to 0.9. Size against the watt rating with 20–30% headroom. A 1000 VA unit may be only a 600 W device.
Do I need pure sine wave output?
If the connected equipment has a modern power supply with active PFC — most current computers and servers — yes. Simulated sine can cause such supplies to shut down or misbehave on battery, defeating the point of the UPS.
Why did my UPS fail during a power cut?
Almost always the battery: sealed lead-acid packs last three to five years, less in warm locations, and degrade silently. Periodic self-tests and scheduled replacement — not waiting for failure — are what keep a UPS honest.
Can I plug a laser printer into a UPS?
No — the fuser draws brief pulses of near-kilowatt power that overload typical UPSs and can trip or damage them. Printers, heaters and motor loads belong on the wall or a surge strip, not on battery-backed outlets.
Should the UPS connect to my computer?
Yes — via USB or network, so the computer can save work and shut down automatically when the battery runs low during a long outage. Without the link, the UPS only postpones an ungraceful shutdown rather than preventing it.
Ride through the blink
From desktop units to rack systems and the DIN-rail DC side of the same problem — with the replacement batteries and testers that keep them ready.
Browse UPS units
View power supplies