Contactor selection for motor switching

Published on 17 July 26

Undersized contactors are one of the most common causes of premature failure in motor circuits — and the mistake usually happens at specification, not installation, because the headline current rating on a contactor is not the rating that matters for a motor. Whether you're building a panel, replacing a welded unit or standardising a stores list, contactor selection comes down to a handful of decisions made in the right order. This guide walks through them.

Short answer

Size a motor contactor by its AC-3 rating in kW against the motor's rated power — never by the AC-1 amp figure, which assumes a resistive load and can be three times more generous. Match the coil to your control voltage, add the auxiliary contacts your control logic needs, and remember a contactor provides no protection at all: pair it with an overload relay sized to the motor's full-load current, with short-circuit protection upstream.

What makes a contactor different from a relay?

Both are electrically operated switches, but a contactor is built for the abuse of power switching: heavier contacts with arc chutes to break motor currents, coils designed for continuous energisation, and standardised mounting for DIN rail and panel layouts. The practical dividing line sits around 10 A — below it, general-purpose relays handle control and light power duty; above it, and for anything three-phase, the job belongs to a contactor. Contactors are also almost always fitted with normally open main contacts that drop out on supply failure — which is exactly what you want, since a motor that restarts itself after a power cut is a hazard, not a convenience.

AC-1 vs AC-3: the rating that catches people out

Every contactor datasheet quotes multiple ratings for the same device, defined by IEC 60947 utilisation categories — and the difference between them is not small:

CategoryDuty it describesWhat the contacts endure
AC-1Resistive loads — heating, distributionMaking and breaking at roughly rated current
AC-3Squirrel-cage motors, breaking while runningMaking at 6–8× rated current (starting inrush), breaking at rated current
AC-4Motors with inching, jogging or plug reversingMaking and breaking at starting current — the hardest duty
DC-13DC electromagnets and solenoidsBreaking inductive DC with no zero-crossing to quench the arc

The same contactor might carry 32 A at AC-1 but only 12 A — perhaps 5.5 kW — at AC-3. Specify from the AC-1 column for a motor and the contacts will be making six times their real rating at every start; welded contacts follow in months. The rule is simple: motors are sized at AC-3 (in kW, matched to the motor's rated power at your supply voltage), and anything that jogs, inches or reverses frequently — hoists, machine tools, roller doors — steps up to AC-4, which in practice means a physically larger contactor than the motor power alone suggests.

Working through a specification

Main contacts. Start from the motor's rated power and full-load current (FLC) from its nameplate, and select the contactor whose AC-3 rating meets or exceeds it at your supply voltage. Three-pole is standard for three-phase motors; four-pole versions suit systems switching neutral or dual circuits. If the duty cycle is severe — more than around 30 starts an hour — size up or check the manufacturer's electrical life curves, because contact life is quoted in operations at rated duty and falls quickly beyond it.

Coil voltage. The coil is specified separately from the contacts and must match the control circuit, not the load: 24 V DC is the modern default for PLC-controlled panels, with 110 V and 230 V AC common in older and simpler installations. Two details matter here. AC coils draw a large inrush when energising (several times their holding current), which counts against small control transformers. And coils driven from PLC or transistor outputs should be fitted with a surge suppressor — an RC snubber or varistor module clipped across the coil — to stop switching transients feeding back into the control electronics.

Auxiliary contacts. Most contactors take clip-on auxiliary blocks providing extra NO and NC contacts for the control circuit: a latching (hold-in) contact for start/stop pushbutton circuits, status indication back to the PLC or panel lamps, and electrical interlocking between reversing pairs. Specify these at the same time as the contactor — retrofitting a panel because one NC contact is missing is a job nobody enjoys.

A contactor is not protection

This is the point most often misunderstood outside panel-building: a contactor switches; it does not protect. Motor protection is a separate function, conventionally split two ways. The thermal overload relay, mounted directly beneath the contactor and dialled to the motor's FLC, trips the coil circuit on sustained overcurrent — a stalled rotor, a lost phase, a jammed drive. Short-circuit protection comes from fuses or a motor-rated circuit breaker upstream. The complete assembly — isolation, short-circuit protection, contactor, overload — is what a direct-on-line (DOL) motor starter packages into one unit, which is often the more economical specification for standalone motors than assembling the parts individually.

One boundary worth knowing: if the application needs speed control, frequent smooth starts or controlled deceleration, the answer stops being a bigger contactor and becomes a drive — see inverters and soft starts. A contactor still usually sits upstream for isolation, but it should never be doing the starting work an electronic starter is built for.

Why contactors fail in service

For maintenance teams, the failure modes map neatly back to specification and supply. Chattering or buzzing — rapid pull-in and drop-out — is almost always coil undervoltage: a sagging control supply, an undersized control transformer, or a poor connection in the coil circuit; the arcing it causes will weld contacts if left. A steady hum on an AC coil points to dirt on the magnet faces or a broken shading ring. Welded main contacts — the motor won't stop — trace back to undersizing, AC-4 duty on an AC-3 device, or repeated starts into a fault. Coil burnout follows sustained over- or under-voltage, or an armature prevented from fully closing, which leaves the coil drawing inrush current continuously. When replacing a failed unit, match the AC-3 rating, coil voltage and auxiliary configuration rather than the brand's catalogue number alone — and if the same unit has failed twice, the specification is the suspect, not the product.

Specifying a panel or replacing a failed unit?

Rapid stocks contactors, overloads and starters from Schneider Electric and more, across coil voltages and frame sizes — with same-day despatch on warehouse-stocked lines.

Specifying contactors

What is the difference between AC-1 and AC-3 ratings?

AC-1 rates the contactor for resistive loads making and breaking at rated current; AC-3 rates it for squirrel-cage motors, where contacts make at six to eight times rated current on every start. The same device carries a much lower AC-3 rating — always size motor duty from the AC-3 column.

Can I use a contactor on a single-phase motor?

Yes — wire the supply through two poles of a standard three-pole contactor (or use a dedicated single-phase unit), sized against the motor's AC-3 rating at 230 V. Single-phase motors draw proportionally higher currents than three-phase equivalents of the same power, so check the FLC rather than assuming from kW.

Do I still need an overload relay if the circuit has an MCB?

Yes. An MCB protects the cable against short circuits and gross overloads; it responds far too slowly to protect a motor from a stall, lost phase or sustained mechanical overload. The thermal overload relay, set to the motor's full-load current, is what saves the winding.

What causes a contactor to chatter?

Coil undervoltage — from a sagging control supply, undersized control transformer or a high-resistance connection in the coil circuit. Fix it promptly: every chatter cycle arcs the main contacts, and prolonged chattering welds them.

Which coil voltage should I specify?

Match the control circuit: 24 V DC is standard for PLC-driven panels and safest for personnel; 110 V AC suits many machine control circuits; 230 V AC remains common in simple installations. The coil voltage is independent of the load voltage — a 24 V DC coil happily switches a 400 V three-phase motor.

Can Rapid supply the full starter assembly?

Yes — alongside contactors, Rapid stocks matching overloads and motor protection, complete motor starters and the wider motor control range, so a panel build or a like-for-like replacement can be ordered in one place.

Share

Post a Comment



Trustpilot