Choose a thermocouple for wide temperature ranges and harsh environments, an RTD for accuracy and long-term stability, and a thermistor for high sensitivity over a narrow range at low cost. That's the one-line version — but real selection decisions turn on drift rates, wiring, response time and what your instrumentation already accepts, and that's where specifications get missed. This guide covers the trade-offs that matter when you're specifying for production, maintenance or the lab bench.
TL;DR:
- Thermocouples cover roughly −200 °C to +1,260 °C (Type K), survive vibration and thermal cycling, and cost little — but drift 1–2 °C per year and need compensating cable, not copper, for any extension run.
- RTDs (Pt100/Pt1000) hold ±0.1–0.5 °C with minimal drift, making them the default for process control and anything audited — at higher cost and slower response.
- Thermistors deliver the highest sensitivity of the three within roughly −50 °C to +150 °C, ideal for embedded monitoring and protection circuits, but their output is non-linear and they self-heat if over-driven.
- Most selection mistakes aren't about the sensing element — they're about wiring, cold junction compensation and matching the sensor to the instrument input.
How do the three technologies actually differ?
Each measures temperature through a different physical effect, and the effect dictates the behaviour. A thermocouple generates a small voltage (around 41 µV/°C for Type K) from the junction of two dissimilar metals — no excitation needed, nothing to burn out at the tip, which is why it tolerates temperatures that would destroy the other two. An RTD exploits the precise, near-linear increase in resistance of platinum with temperature: a Pt100 reads 100 Ω at 0 °C and rises predictably from there. A thermistor is a ceramic semiconductor whose resistance changes steeply and non-linearly with temperature — that steepness is what gives it sensitivity an RTD can't match over small spans.
For deeper dives on two of the three, see our guides to K-type thermocouples and where thermistors fit in temperature sensing — this article is about choosing between them.
Thermocouple vs RTD vs thermistor at a glance
| Thermocouple (Type K) | RTD (Pt100) | Thermistor (NTC) |
| Typical range | −200 to +1,260 °C | −200 to +600 °C | −50 to +150 °C |
| Accuracy | ±1.5–2.5 °C (Class 1–2) | ±0.1–0.5 °C (Class A–B) | ±0.1–1 °C within band |
| Long-term drift | 1–2 °C per year | Very low | Low if glass-sealed; higher if epoxy-coated |
| Response time | Fast — exposed junctions in fractions of a second | Slower — larger thermal mass | Fast in bead/chip form |
| Linearity | Reasonable; standardised tables | Excellent | Strongly non-linear |
| Excitation required | None — self-generating | Yes — measurement current | Yes — measurement current |
| Ruggedness | Excellent; handles vibration and cycling | Good sheathed; element is delicate | Good encapsulated; sensitive to moisture |
| Relative cost | Low | Higher | Lowest |
Which requirement should drive the decision?
If range rules, it's a thermocouple. Above roughly 300 °C the other two are out of contention, and above 600 °C it's thermocouples only — furnaces, ovens, exhausts, heat treatment. Below that ceiling, the thermocouple's other virtues are ruggedness and price: on a machine that vibrates, in a probe that will be dropped, or anywhere sensors are treated as consumables, Type K is the pragmatic default.
If accuracy and auditability rule, it's an RTD. A Class A Pt100 holds tolerances a thermocouple can't sustain, and — critically for regulated environments — holds them year after year. Where readings feed HACCP records, pharmaceutical process logs or calibration-controlled test equipment, the RTD's low drift means longer recalibration intervals and fewer out-of-tolerance findings. The price is slower response and a more delicate element, so specify a sheathed probe for anything industrial.
If sensitivity or integration rules, it's a thermistor. Within a ±50 °C band around its nominal point, an NTC thermistor resolves smaller changes than either alternative, in a package small enough to embed on a PCB, in a battery pack or inside a motor winding. For protection rather than measurement — tripping at an overtemperature threshold — a PTC thermistor switches sharply and repeatably. The constraint is the narrow band and the non-linear curve, which your electronics must linearise.
Where do temperature sensor installations go wrong?
The element is rarely the weak point — the installation is. Four failures account for most callbacks:
Copper extension on a thermocouple. Extending thermocouple wiring with standard copper cable creates new junctions of dissimilar metals at the joint, each generating its own voltage. The reading shifts unpredictably with ambient temperature at the connection point. Always extend with the matching compensating cable and connectors for the thermocouple type.
Ignoring lead resistance on a 2-wire RTD. A Pt100 changes roughly 0.385 Ω/°C, so even a few metres of cable adds resistance the instrument reads as temperature — easily several degrees of error. Use 3-wire connection as the industrial minimum; 4-wire where the accuracy actually matters. Or specify Pt1000, where lead resistance is a tenth of the problem.
Thermistor self-heating. Push too much measurement current through a thermistor and it warms itself above the medium it's measuring, reading permanently high. Check the dissipation constant against your excitation current, especially in still air.
Drift treated as failure — or failure treated as drift. A thermocouple reading a few degrees low after years at high temperature is normal ageing (the "green rot" oxidation on Type K in reducing atmospheres is the extreme case) and a planned-replacement matter. An RTD that has drifted noticeably, by contrast, has usually been mechanically damaged or contaminated — investigate rather than recalibrate around it.
Found the right technology?
Browse thermocouples, thermistors and temperature probes at Rapid — from PCB-mount sensing elements to sheathed industrial probes and handheld instruments.
Specifying temperature sensors
What is the difference between Pt100 and Pt1000?
Both are platinum RTDs with identical accuracy classes; the Pt1000 simply reads 1,000 Ω at 0 °C rather than 100 Ω. The higher base resistance makes cable resistance proportionally less significant, so Pt1000 suits 2-wire connections and battery-powered instruments where measurement current must stay low.
Can I extend a thermocouple with ordinary copper cable?
No. Copper joints against thermocouple alloys create unintended junctions that add error varying with ambient temperature. Use compensating or extension cable matched to the thermocouple type, with matching plugs and sockets, all the way back to the instrument's cold junction.
Why do thermocouples drift over time?
Sustained high temperature gradually changes the alloy composition at the measuring junction, shifting its output — typically 1–2 °C per year, faster with thermal cycling or reducing atmospheres. Build replacement into maintenance schedules for critical measurement points rather than waiting for readings to wander.
Which sensor is best for a school or university lab?
Type K thermocouples with handheld meters are the workhorse: wide range, robust enough for student handling, and probes are inexpensive to replace. For fixed experiments needing precision — calorimetry, for instance — a Pt100 bench instrument gives more defensible results.
Do I need a transmitter with an RTD or thermocouple?
Not always — many controllers and panel meters accept sensor inputs directly. Fit a head-mounted transmitter when cable runs are long, electrical noise is high, or your control system standardises on 4–20 mA inputs; the signal travels far more robustly than millivolts or ohms.
Can Rapid supply matching probes and instruments together?
Yes — alongside sensing elements in temperature sensors, thermistors and thermocouples, Rapid stocks thermocouples and probes for test instruments, so probes, plugs and meters can be ordered in one place.