18650 batteries: the specs that actually matter

Published on 28 July 26

The 18650 is the workhorse lithium-ion cell — 18 mm across, 65 mm long, and behind everything from torches and vapes to power tool packs, e-bikes and portable instruments. The catch is that every 18650 looks identical, yet they behave very differently: two cells the same size can differ threefold in how hard they can be driven, and the wrong choice means either a device that runs flat too soon or one that struggles under load. Choosing well comes down to four things — capacity, discharge current, terminal type and whether the cell is protected — plus one that matters more than any of them: buying a genuine cell.

Short answer

If you want the longest runtime, choose a high-capacity cell such as the Samsung INR18650-35E or Panasonic NCR18650GA (around 3450 mAh). If the device draws heavy current — power tools, high-output torches, regulated mods — choose a high-drain cell such as the Samsung INR18650-25R or 30Q. Match the terminal type to your holder, and only ever buy genuine, correctly rated cells.

How the cells compare

Every cell below is a 3.6–3.7 V lithium-ion 18650. What separates them is the balance between how much energy they store and how fast they can deliver it — the two figures pull against each other, so the right cell depends entirely on the load.

Cell Capacity Discharge character Best for
Samsung INR18650-35E 3450 mAh High capacity, moderate current Maximum runtime — instruments, packs, torches
Panasonic NCR18650GA 3450 mAh High capacity, moderate current Runtime with a little more headroom on current
Samsung INR18650-30Q 3000 mAh Balanced — good capacity and current All-rounder where the load is unknown
Samsung INR18650-25R 2500 mAh High drain Heavy, sustained current draw
Panasonic NCR18650B 3400 mAh Very high capacity, low current Long runtime at gentle loads

Capacity or current: the trade-off that decides it

This is the single most important thing to understand about 18650 cells, and it is where most wrong purchases happen. Capacity, in milliamp-hours, is how much energy the cell holds — its runtime. The maximum continuous discharge current, in amps, is how fast it can deliver that energy without overheating. The chemistry that maximises one compromises the other, so no 18650 is best at both.

At the extremes the difference is stark. A high-capacity cell like the 35E stores around 3450 mAh but is typically rated for a continuous discharge in the region of 8 A; a high-drain cell like the 25R holds less — 2500 mAh — but will deliver roughly 20 A. Ask a high-capacity cell to supply a high-current load and it will sag in voltage, run hot and age quickly; fit a high-drain cell where you only needed runtime and you have simply paid for capacity you threw away. The practical rule: size the cell to the load's current draw first, then take whatever capacity that leaves you. Published discharge ratings vary in how they are measured, so always confirm the figure on the manufacturer's datasheet for the exact cell.

Flat top or button top?

The terminal is a physical fit question, not a performance one. A flat-top cell has a level positive end; a button-top cell has a small raised nub. Series battery holders and many torches need the button top to make contact and to bridge cell-to-cell, so a flat-top cell may simply not connect. Spot-welded packs and many purpose-built devices, on the other hand, are designed around flat tops. Check what the device or holder expects before ordering — it is the most common reason a correctly specified cell still will not work. The Sanyo UR18650ZM2, for instance, has a flat-top cell.

Protected or unprotected?

A protected 18650 carries a tiny circuit board at one end that guards against over-discharge, over-charge and short circuit, cutting the cell off before it reaches a dangerous state. That protection adds two to three millimetres of length, which can stop a protected cell fitting a tight holder, and it caps the current, which rules protected cells out of genuine high-drain use.

The distinction follows the application. A single cell in a torch or a standalone device is safer as a protected cell. Cells destined for a multi-cell pack are almost always unprotected, because the pack has its own battery management system doing the same job more comprehensively — and because per-cell protection boards would interfere with balancing. If you are building a pack, that BMS is not optional; unprotected cells with no management system are where lithium batteries become genuinely hazardous.

Should you consider a 21700 instead?

The 21700 is the 18650's larger successor — 21 mm by 70 mm — and it is increasingly the cell of choice for new designs because the extra volume buys both more capacity and more current in one step. The Samsung INR21700-50E reaches around 4900 mAh, and the 40T pairs 4000 mAh with a high discharge rating. It is not a drop-in for an 18650 — the cell is physically larger and will not fit an 18650 holder — but if you are designing from scratch rather than replacing a cell, it is worth comparing before committing to the older format.

What should you check before buying?

Five checks. First, current: establish the load's continuous draw and choose a cell rated comfortably above it. Second, capacity: take the highest capacity that current rating allows. Third, terminal: flat top or button top, matched to the holder or device. Fourth, protection: protected for a single loose cell, unprotected only where a BMS manages the pack. Fifth, chemistry and voltage: standard 18650s are 3.6–3.7 V lithium-ion, but lithium iron phosphate cells are not interchangeable on voltage. And underpinning all of it: buy genuine cells from a known supplier. The 18650 market is awash with rewrapped cells claiming capacities no 18650 can physically reach; a genuine Samsung, Panasonic or LG cell performs to its datasheet and is safe to charge, which a counterfeit is not.

Browse rechargeable cells

Genuine 18650 and 21700 cells from Samsung, Panasonic, LG and Sanyo, with holders and chargers to match, stocked for next-day UK delivery.

Frequently asked questions

What does mAh mean on an 18650 cell?

Milliamp-hours measure the cell's capacity — roughly how much energy it stores, and therefore how long it lasts between charges. A higher figure means longer runtime, but capacity has to be weighed against how much current the cell can safely deliver, which usually falls as capacity rises.

Which 18650 has the highest capacity?

Among current cells, the highest capacities sit around 3400–3500 mAh — the Samsung INR18650-35E and Panasonic NCR18650GA are examples. Cells claiming much more than that are not genuine; the chemistry of an 18650 has a physical ceiling.

Do I need a protected or unprotected 18650?

For a single cell used loose in a torch or device, a protected cell is the safer choice. For a multi-cell pack, use unprotected cells managed by a proper battery management system — the BMS provides the protection, and per-cell boards would get in the way of balancing.

Can I replace an 18650 with a 21700?

Not directly — a 21700 is physically larger and will not fit an 18650 holder or device. It offers more capacity and current, so it is worth considering for a new design, but it is a redesign rather than a straight swap.

Share

Post a Comment



Trustpilot