Sign in to your account to see your Schools Discount Scheme pricing

Ultimate guide to soldering equipment

Written by Tom Hanmore, Digital Marketing Executive Published on 21 August 25

What is soldering?

Soldering, in its simplest form, is joining metal parts together using heat and a fusible alloy known as ‘solder’. It’s a technique you’ll find in nearly every electronic device, look inside a circuit board and you’ll see countless soldered joints holding components in place.

While soldering is often associated with electronics, it’s a method used across industries, from automotive and aerospace to plumbing and jewellery. It’s not just about making connections; it’s about making them reliable, conductive and durable.

Interestingly, soldering isn’t a modern invention. The technique dates back over 5,000 years, with early examples found as far back as 4,000 BC. Of course, the tools and materials have evolved dramatically since then. A major turning point came in 1986 with the introduction of the first electric soldering iron, paving the way for the tools we rely on today.

Fast forward to the present and soldering has become a cornerstone of modern manufacturing and repair. With advanced equipment from brands like Weller, professionals can now achieve cleaner joints, tighter tolerances and safer working conditions than ever before.

Why Weller is the industry leader

Weller has pioneered the art and science of professional hand soldering. Today, more than ever, the brand is focused on what it truly means to be #PowerfulTogether. From electronics manufacturing to medical and defence, Weller tools are trusted by professionals for their performance and durability.

Founded in 1945 by Carl E. Weller, who pioneered the transformer-based instant heating soldering method, Weller has consistently led the way in hand-soldering technology. Today, the brand continues to evolve, offering a complete ecosystem of tools designed to meet the demands of modern workbenches.

Weller doesn’t just make soldering irons. It “owns the bench,” providing everything from advanced soldering and rework stations to fume extraction units, precision hand tools and soldering accessories. Whether you're working on industrial-scale production or fine electronics assembly, Weller’s product range is built to support every stage of the process.

Their commitment to innovation is evident in solutions like the WXsmart platform, which integrates IoT connectivity, tip recognition and digital control for smarter, safer soldering. Weller also supports the shift toward Industry 4.0, ensuring its tools are ready for connected, data-driven environments.

The brand’s reputation is built on more than just product quality. Weller’s tools are engineered with the user in mind - offering ergonomic designs, fast heat-up times and intuitive interfaces that make even complex tasks more manageable. Their 80 Years Limited Black Edition series is a testament to this legacy, combining sleek design with cutting-edge performance.

Weller 80 Years Limited Black Editions
Weller 80 Years Limited Black Editions

Whether you're outfitting a new bench or upgrading your current setup, Weller provides the tools and technology to help you solder with confidence, today and into the future.


Soldering essentials

Whether you're setting up a new production line, maintaining equipment or refining your bench for precision rework, having the right soldering tools is essential to achieving consistent, high-quality results.

We’ve curated a list of core equipment that supports efficient workflows and reliable performance across industrial and technical environments. The great thing about soldering is that it doesn’t take much to get started - just the right tools and a solid understanding of the process.

Soldering iron/station

Weller ET Series Tips
ET Soldering Tip Set

A soldering iron is an essential tool for joining electronic components and its performance often comes down to the tip you use. The Weller ET Series Tips are a great choice for professionals, offering reliable heat transfer and precision across a wide range of applications.

Designed for flexibility, these tips are easily swappable and perfectly suited for delicate soldering work, as well as larger joints. At Rapid, we’re proud to be one of the few major distributors currently stocking these genuine Weller tips, making sure you maintain consistency across your operation.

Weller WE1010 Soldering Station
WE1010 Soldering Station "Black Edition"

To get the most from your ET Series Tips, pair them with the Weller WE1010 Soldering Station. With excellent temperature stability, digital control and an ergonomic design, the WE1010 supports repeatable, high-quality results in demanding environments, whether it be working on prototypes or batch production.

Solder wire

Solder wire is the filler metal that melts to form the electrical connection between components. In industrial and electronics manufacturing, lead-free solder with a rosin core is commonly preferred for compliance and clean joint formation. Selecting the right diameter is key - finer wire for precision work, thicker wire for larger joints.

Weller’s WSW solder wire is designed to optimise performance across all soldering tasks. With reduced splash, a guaranteed continuous flux core and high-purity metal, it delivers durable, crack-resistant joints, even on challenging surfaces.

We also provide our own soldering wire through our own brand, R-TECH - an affordable, high-quality alternative with plenty of types to choose from:

100g reel
100g Reel
500g reel
500g Reel
12g tube
12g Tube

Flux

Flux helps clean the metal surfaces and improves solder flow. It’s especially useful when working with oxidised components or during rework. Available in paste, liquid or pen form, flux is a must-have for clean, reliable joints and helps reduce defects in production environments.

For those seeking professional-grade performance, Weller Electronic Flux is a standout option. This halogen-free, colophony-based liquid flux promotes fast and efficient soldering of electronic components and is also suitable for tin plating and solder-pot-dip applications. After soldering, the flux remains on the joint and should be removed with a suitable cleaner if a flux-free board is required, ideal for high-spec or sensitive environments.

Browse full range
Weller Electronic Flux
Additional flux example

Weller WXDP 120 Desoldering Iron
Additional desoldering tool

Desoldering tools

Even in well-controlled settings, rework is a necessary part of electronics manufacturing and repair. Whether you're correcting misaligned components or removing excess solder, having the right equipment ensures you can make adjustments without damaging the board.

For basic rework, tools such as solder suckers (pumps) and desoldering braid offer quick, effective solutions. For more demanding applications, a high-performance tool like the Weller WXDP 120 Desoldering Iron offers serious advantages. Delivering 120 watts of power at 24 volts, it’s designed for efficient solder removal in professional and industrial environments. Typical uses include circuit board rework, component replacement and precision repair tasks where speed and control are essential.

Investing in the right desoldering equipment helps reduce rework time, prevent damage and maintain quality standards across production and service operations.

Browse full range

Safety gear

Safety should always be a priority when soldering, especially during extended sessions where tasks are repetitive, prolonged or performed in enclosed workspaces. Basic protective gear like heat-resistant gloves, safety glasses and a stable iron stand helps prevent burns and accidental contact.

However, for manufacturing teams and technicians working in high-volume or continuous soldering operations, air quality becomes just as important. Soldering produces smoke, vapours and fine particulate matter that can pose long-term health risks if not properly managed. That’s where fume extraction comes in. A reliable extraction system helps maintain a clean, breathable workspace and supports workplace safety standards.

One standout solution is the Weller 80 Years Limited Black Edition ZeroSmog Shield - an air purification unit designed specifically for soldering in labs, workshops,and manufacturing environments. It uses a combination of EPA E10 filters for particulates and activated carbon for gases, capturing harmful solder fumes before they spread.

Browse full range
Safety goggles
Fume extractor

Take the next step in soldering

Soldering doesn’t have to be complicated. With the right tools, proven techniques and guidance from trusted brands like Weller, manufacturers and industry professionals can achieve clean, consistent results across a wide range of production and repair applications.

From selecting the right soldering station and tip to mastering desoldering and flux use, this guide has outlined the essentials to help you streamline workflows and maintain high standards. Weller’s commitment to precision, safety and innovation continues to set the benchmark, whether you're assembling prototypes, repairing PCBs or managing high-volume production lines.

Ready to optimise your soldering setup? Explore our full range of Weller soldering equipment or get in touch with one of our specialists who can help your business grow, thrive and move forward successfully.

Share

Post a Comment



Trustpilot