MPU6050 alternatives: what to use now the chip is EOL

Published on 08 July 26

The MPU6050 motion sensor module has been the default six-axis IMU for a decade of Arduino, Raspberry Pi and micro:bit projects — a three-axis gyroscope and three-axis accelerometer on one chip, talking over I²C, for a few pounds. The search for alternatives has a real driver behind it: TDK InvenSense has discontinued the MPU-6050 chip and no longer recommends it for new designs. That doesn't mean modules are disappearing — they remain widely manufactured and stocked — but it does change which sensor makes sense depending on what you're building.

Short answer

For education and prototyping, the MPU6050 module remains a perfectly good buy with unmatched tutorial support. If the project only uses tilt, tap or vibration sensing, a plain accelerometer such as the ADXL345 does the job on current-production silicon. For genuine orientation tracking, the Adafruit BNO055 is the meaningful upgrade — it computes orientation on-chip, which is the part the MPU6050 makes you do yourself.

How the alternatives compare

The MPU6050's substitutes aren't all the same kind of product, because MPU6050 projects don't all use the same parts of it. Many only ever read the accelerometer; some need the gyroscope for rotation rates; a smaller group needs actual orientation — pitch, roll and heading — which the MPU6050 alone can only estimate through filtering code, since it has no magnetometer.

Module Sensors Interface Choose it when
Joy-IT MPU6050 3-axis gyro + 3-axis accelerometer I²C Teaching and prototyping, where tutorial and library support matter most
Adafruit ADXL345 3-axis accelerometer, ±2–16 g I²C / SPI Tilt, tap, free-fall and vibration sensing without a gyro
Adafruit LIS3DH 3-axis accelerometer, ±2–16 g I²C / SPI Low-power motion sensing in battery projects
Adafruit BNO055 Accelerometer + gyro + magnetometer, fused on-chip I²C Absolute orientation output — pitch, roll and heading — without writing fusion code
Arduino Nano 33 BLE Rev2 9-axis IMU on the board itself Onboard New builds where controller and IMU can be one purchase and zero wiring

Is the MPU-6050 discontinued?

The chip is — TDK InvenSense ended production and lists it as not recommended for new designs. The modules built around it are a different matter: they continue to be manufactured in volume and remain easy to buy and nothing about the discontinuation makes existing boards worse at what they do. The practical reading is straightforward. For classroom sets, one-off projects and prototypes, the MPU6050's decade of tutorials, wiring diagrams and library support still makes it the easiest six-axis sensor to get working. For a product design with a multi-year production life, building on a discontinued chip carries sourcing risk that current-production alternatives avoid.

Do you actually need the gyroscope?

A surprising share of MPU6050 projects never read the gyro. Tilt detection, orientation switching, tap and shake detection, vibration monitoring, free-fall alarms — all of these are accelerometer jobs and a dedicated accelerometer does them on current silicon with simpler code. The ADXL345 has tap, double-tap and free-fall detection built into the chip itself, so events arrive as interrupts rather than maths. The LIS3DH covers the same ground with very low power draw, which suits battery-powered and wearable builds. If your sketch only ever uses the accelerometer readings, either of these is a cleaner substitute than another six-axis part.

What's the step up for orientation sensing?

The MPU6050's hardest problem was never the hardware — it was turning raw gyro and accelerometer readings into a stable orientation, which means complementary or Kalman filtering, drift handling and no absolute heading at all without a separate magnetometer. The BNO055 removes that entire layer: it carries all three sensor types plus a processor running the fusion algorithms and simply outputs orientation as Euler angles or quaternions over I²C. For robotics, camera stabilisation, heading-aware projects — anything where orientation is the goal rather than raw motion data — it replaces both the MPU6050 and the filtering code around it.

Boards with the IMU built in

For a new build there's also the option of not wiring a sensor module at all. The Arduino Nano 33 BLE Rev2 carries a nine-axis IMU on the board alongside a Cortex-M4 and Bluetooth, with official library support — a tidy route for wearables, motion controllers and gesture projects where the MPU6050 would have been the first purchase and the microcontroller the second.

What should you check before substituting?

The main cost of moving off the MPU6050 is software, not wiring. Every module here speaks I²C at 3.3 V logic, but the registers and libraries are entirely different, so existing MPU6050 code does not port — budget for swapping the library and reworking the readout and check library support for your platform (Arduino coverage is universal; micro:bit MakeCode support varies by sensor). Beyond that: confirm the measurement ranges suit the application, check the axis orientation printed on the new board against your mounting and if heading matters, remember only the magnetometer-equipped options can provide it — and they'll want calibrating away from motors and magnets.

Browse motion and sensor boards

Accelerometers, IMUs and sensor breakouts from Adafruit, Joy-IT, Seeed and more, ready for Arduino, Raspberry Pi and micro:bit.

Frequently asked questions

Is the MPU6050 still worth buying?

For learning and prototyping, yes — modules are still made in volume and no other six-axis sensor comes close to its depth of tutorials and example code. The discontinuation matters mainly for product designs that need a supply of the chip for years to come.

What is the direct successor to the MPU-6050?

TDK InvenSense's own successors are its ICM series of six-axis sensors. At module level, though, substitution is rarely one-for-one — the better question is whether the project needs an accelerometer, a full IMU or computed orientation, because each points to a different board.

Can the MPU6050 measure heading like a compass?

No — it has no magnetometer, so it cannot sense absolute heading and gyro-based heading estimates drift over time. Projects that need real heading want a nine-axis sensor such as the BNO055.

Will my MPU6050 code work with a replacement sensor?

The wiring usually carries over — these are all I²C devices — but the code will not. Each sensor family has its own registers and libraries, so plan to swap the library and adapt the readout rather than reuse the sketch unchanged.

Share

Post a Comment



Trustpilot