High-integrity signal conditioning: why your choice of signal converter matters in hazardous areas

Published on 17 June 26

In industrial automation, a reliable 4–20mA loop is essential for keeping systems running safely and consistently. In hazardous environments, such as Zone 0 and Zone 1 areas, signal converters do far more than simply translate data. They play an important role in maintaining signal reliability while helping protect both equipment and personnel.

Why galvanic isolation matters

Electrical noise and ground loops can quietly affect measurement accuracy and system performance. A good-quality signal converter with galvanic isolation helps prevent these issues by separating the input and output circuits electrically.

This helps to:

  • Prevent common-mode voltage from affecting PLC or DCS performance
  • Contain surge events, reducing the chance of faults spreading through the control cabinet
  • Maintain signal accuracy over longer cable runs by reducing unwanted electrical interference

I0 demanding industrial environments, these protections can make a significant difference to overall system reliability.

Preserving HART® communication

One issue often overlooked when selecting signal converters is whether they support HART® communication. Some standard converters unintentionally block the high-frequency digital signals used for diagnostics and device communication.

HART transparency allows both analogue and digital signals to travel together over the same 4–20mA loop. This means maintenance teams can still access device diagnostics, carry out remote calibration and monitor valve positioners without disrupting normal operation.

Choosing a suitable converter, such as the Weidmüller 2456160000 Signal Converter, can help ensure compatibility with FDT/DTM software, improving visibility between field devices and the control room.

SIL ratings and compliance

For engineers and operations teams, reducing risk is always a priority. A signal converter with a documented SIL 2 rating, in line with IEC 61508, provides added confidence for use in safety-instrumented systems (SIS).

Devices with strong reliability figures and long service life can also help reduce maintenance requirements and lower long-term costs across an installation.

Built for long-term reliability

Choosing the right signal converter is about more than matching input and output signals. Factors such as installation speed, certification and long-term performance all matter.

Features such as PUSH IN connection technology can simplify wiring and reduce commissioning time, while ATEX and IECEx approvals help ensure suitability for hazardous environments. Combined, these considerations can improve reliability and reduce the risk of signal issues caused by vibration or poor connections.

Share

Post a Comment



Trustpilot