For over two decades, LEGO MINDSTORMS has inspired those of all ages to test and build their confidence with technology through play. By combining the LEGO building system with robotic and coding elements, builders can create anything they can imagine, while developing the STEM skills that 7 in 10 parents say are essential to their child's future success.
This latest evolution of the much-loved theme continues this commitment to helping children develop STEM skills in a fun and exciting way at home.
The new LEGO MINDSTORMS Robot Inventor 5-in-1 model gives builders aged 10+ the power to bring one of the set's five unique designs to life or take their own builds to the next level by programming them to walk, talk, think and do more than ever before. Kids can also code their own remote-control features for the models in the LEGO MINDSTORMS Robot Inventor app or connect their own controllers to the app using Bluetooth.
5 unique models to build and code - the largest robot 'Blast' stands at over 360mm (14in.) tall .The free LEGO® MINDSTORMS® Robot Inventor coding app for kids uses coding language based on Scratch and supports Python for more advanced coders. The application works across PC Windows 10 + macOS, iOS and Android tablets and smartphones as well as specific Fire OS devices.
New elements:
- The new Intelligent Hub is an advanced yet simple-to-use device featuring 6 input/output ports for connecting a variety of sensors and motors. The Hub can also be used with LEGO Technic and System elements to create fun robots, dynamic devices and other interactive models
- LED 5x5 matrix
- Bluetooth connectivity
- 6-axis gyro/accelerometer
- Includes a micro USB port for connectivity with compatible devices
- Speaker
- Rechargeable Lithium-ion battery included
- Colour sensor – able to distinguish between eight colours and measures reflected and ambient light from darkness to bright sunlight
- Distance sensor – detects obstacles, programmable LED 'eyes' and an integrated 6-pin adaptor for third-party sensors, boards and DIY hardware
- 4 x medium-angular motors feature low-profile design, integrated rotation sensor with absolute positioning
- New 7 x 11 teal baseplate
- New black wheels
- New frames
- 5 models to build (one at a time)
- Ages 10+
- 949 pieces
- LEGO type 51515
Age Range |
10+ |
Material |
Plastic |
Number of Pieces |
949 |
Type |
Lego Mindstorms |
To use this facility please Sign In. Alternatively use our Quotation page.
Sign In