13 October 26
By the Rapid technical team Updated October 2026
The best multimeter in the UK depends on the job you do. For engineering, automotive and EV diagnostics, Gossen Metrawatt's METRAHIT multimeters ...Read the full story
30 September 26
In short
More than 70% of Raspberry Pi boards now go into industrial and embedded products, not hobby projects.
Sony uses Raspberry Pi to monitor its production lines, at a fractio...Read the full story
29 September 26
Coach bolts and coach screws get muddled more than almost any other fixing - the names are nearly the same, they're both big, both heavy-duty, and both live in the timber and structural end of the too...Read the full story
29 September 26
Every controlled door is really answering one question, over and over: should this person be allowed in? A door entry system answers it for you - letting the right people through and keeping everyone ...Read the full story
29 September 26
The consumer unit is the quiet hub of a building's electrics - the modern fuse board where the incoming supply splits out to every circuit, and where the protection that keeps those circuits (and the ...Read the full story
28 September 26
Anyone who works on their knees knows the feeling: an hour into a job on a hard floor and every shift of weight is a small negotiation with your joints. Knee pads fix that - and they're one of those b...Read the full story
28 September 26
Tip two boxes of screws onto the bench and a self-tapping and a self-drilling screw look almost like twins. Pick the wrong one, though, and the job tells you soon enough - a screw spinning uselessly i...Read the full story
28 September 26
A ratchet strap only has one job: to keep a load exactly where you put it, however the road, the ferry or the forklift tries to move it. Get it right and you forget it's even there. Get it wrong - the...Read the full story
04 September 26
Buying a headset ought to take five minutes. Then you open the category page, meet forty near-identical black earpieces, and every single one swears it has crystal-clear audio and all-day comfort. Twe...Read the full story
26 August 26
Great supplier relationships are a big part of how we help customers get the right result. At Smart Manufacturing Week, three of the brands we work with — FLIR, Brainboxes and CRC Indu...Read the full story
26 August 26
Alongside the thousands of exceptional products we stock at Rapid, we also design and back our own exclusive brands — giving you great-value options across a huge range of categories...Read the full story
07 August 26
Short answer
A logic gate is a building block of a digital circuit that takes one or more binary inputs (0 or 1) and produces a single binary output according to a fixed rule. The seven core ga...Read the full story
04 August 26
PID control is how machines hold a value steady against a world that keeps disturbing it — the oven at temperature as the door opens, the motor at speed as the load bites, the pressure constant as dem...Read the full story
04 August 26
The short answer
A cable assembly is a cable terminated with connectors at one or both ends — a finished, tested, plug-and-play part rather than raw cable to be cut and terminated on the bench....Read the full story
30 July 26
Fibre optic cable carries data as light down a glass core, guided by total internal reflection — the same physics demonstrated with a torch and a water stream in every school lab, industrialised into ...Read the full story
30 July 26
An uninterruptible power supply does a more modest job than its name suggests, and understanding that is the key to buying the right one. A typical UPS exists to bridge the gap between the mains faili...Read the full story
29 July 26
Joint quality is decided by three things: the iron, the technique and the consumables — and the third gets the least attention while causing a remarkable share of the problems. The solder alloy sets t...Read the full story
28 July 26
A printed circuit board is a laminate sandwich: a fibreglass substrate (almost always FR-4), copper foil etched into tracks, a solder mask that keeps molten solder where it belongs, and a silkscreen l...Read the full story
28 July 26
The 18650 is the workhorse lithium-ion cell — 18mm across, 65mm long, and behind everything from torches and vapes to power tool packs, e-bikes and portable instruments. The catch is that every 18650 ...Read the full story
27 July 26
A potentiometer is a resistor with a third terminal — a wiper that slides along the resistive track — and that one addition makes it two components in one. Use all three terminals and it's a voltage d...Read the full story
27 July 26
The short answer
Choose a connector by asking why the joint needs to separate at all. Every connector is a deliberately engineered break in a circuit — added to make a product easier to build, ...Read the full story