Sign in to your account to see your Special Education pricing

Tektronix launches DPO1 oscilloscope for schools, colleges and universities

Written by Millie Lancaster Published on 10 November 26

Bandwidth, sample rate and channel count still matter. But in a teaching lab, the bigger question is how well an oscilloscope helps students learn. The new Tektronix DPO1 Series (1 Series) is built around that idea, and it's available now from Rapid Electronics, in stock for same-day UK despatch.

12-bit

vertical resolution

200 MHz

maximum bandwidth

1.25 GS/s

sample rate

10M

points per channel

More than a spec sheet: what teaching labs really need

For decades, oscilloscopes have been compared on the same handful of numbers: bandwidth, sample rate, memory depth and channel count. They're still important, but in education they only tell part of the story.

Electronics labs today face very different pressures:

  • Cohorts are bigger
  • Practical teaching time is tighter
  • Embedded systems are more complex
  • Lab space and equipment budgets are limited, but universities still need to prepare students for industry

So the question isn't just "What can this oscilloscope measure?" It's "How well does it help students learn?"

Tektronix DPO1 Series oscilloscope

Less time on the controls, more time on the concepts

Ask any electronics lecturer where lab time goes, and circuit theory is rarely the answer. Much of it goes on helping students find their way around unfamiliar instruments: menus, controls, triggering and measurement functions. That's especially true in first-year modules and multidisciplinary STEM courses, where students arrive with very different levels of confidence.

Students don't come to university to learn oscilloscopes. They learn oscilloscopes to understand electronics.

The DPO1 is designed with that in mind. A 7" capacitive touchscreen, a simplified front panel and an interface that's consistent across the wider Tektronix oscilloscope range mean students get comfortable quickly. That leaves more of the session for what really matters, like signal integrity, timing, filtering and circuit behaviour.

Designed for teaching

Education controls: teach the theory, not the shortcut

Modern scopes can automate almost any measurement at the touch of a button. That's great for efficiency, but it can skip the learning.

The DPO1 lets lecturers switch off Autoset, automatic measurements and cursors, so students work out frequency, amplitude and timing by hand before moving on to automated workflows. You decide how much help the instrument gives.

Built for flexible lab spaces

Oscilloscopes have traditionally lived on a fixed bench. But many engineering departments now use flexible, shared spaces for collaborative and multidisciplinary project work.

The DPO1 has a compact footprint, a built-in carry handle and VESA mounting, so it can go on monitor arms, mobile trolleys, desk mounts or walls. The equipment moves to where the learning is happening.

Beyond the bench: software and remote access

Engineering doesn't stop when a waveform appears on screen. The DPO1 works with TekScope PC analysis software, Python drivers, eScope remote access and KickStart software.

Students can analyse, automate and share their measurements in a way that mirrors professional engineering practice.

DPO1 Series key specifications

Specification DPO1 Series
Analogue channels2 (DPO1xx2) or 4 (DPO1xx4)
Bandwidth50 MHz, 70 MHz, 100 MHz or 200 MHz
Max sample rate1.25 GS/s
Record length10M samples per channel
Vertical resolution12-bit
Trigger typesEdge, pulse width, runt, timeout, rise/fall
Protocol decodeI2C, SPI, UART
DVM / counter5-digit DVM, 7-digit frequency counter
Signal generator25 MHz AFG (S models only)
Display7" or greater capacitive touchscreen
MountingVESA compatible, integrated carry handle
SoftwareTekScope, Python drivers, eScope remote access, KickStart

The DPO1 in universities and colleges

The DPO1 Series is built for undergraduate teaching and project work:

First-year and teaching labs

The touchscreen and education controls help students build confidence and core measurement skills in electronic and electrical engineering and physics.

Final-year and research projects

12-bit resolution, a 10M-point record length, FFT, advanced maths, mask testing and Bode plots make it a capable bench instrument.

Embedded systems courses

I2C, SPI and UART decoding helps students debug the microcontroller designs used in automotive, industrial automation, energy and consumer electronics.

T Levels

Colleges delivering the Engineering and Manufacturing T Level can give learners hands-on experience of industry-standard test equipment.

DPO1 Series FAQs for educators

What is the Tektronix DPO1 Series?

The DPO1 Series, also called the Tektronix 1 Series, is an entry-level digital oscilloscope range with 2 or 4 channels, bandwidths from 50 MHz to 200 MHz and 12-bit vertical resolution.

Can lecturers turn off Autoset and automatic measurements?

Yes. The DPO1's education controls let lecturers disable Autoset, automatic measurements and cursors, so students make measurements by hand and learn the principles behind them.

Which DPO1 model is best for a teaching lab?

For first-year and introductory labs, a 2-channel 50 MHz or 70 MHz model covers most practicals. For embedded systems, power electronics or research work, a 4-channel 100 MHz or 200 MHz model gives more headroom.

Does the DPO1 have a built-in signal generator?

Yes, S models include a 25 MHz arbitrary function generator (AFG) with basic waveforms and modulation.

Can students use the DPO1 to debug microcontroller projects?

Yes. The DPO1 decodes I2C, SPI and UART, common serial protocols on microcontroller boards, so students can see and debug the communication between devices.

Is the DPO1 suitable for university research projects?

Yes. 12-bit resolution, a 10M-point record length per channel and analysis tools including FFT, advanced maths, mask testing and Bode plots make it a capable bench instrument for final-year and postgraduate projects.

Share

Post a Comment



Trustpilot