Scales for industry: types, applications and how industrial weighing scales work

Published on 13 March 26
Set of industry weighing scales

Weighing is a critical process across many industries. From manufacturing and logistics to agriculture and packaging, industrial weighing scales help businesses measure materials accurately, maintain quality control and ensure regulatory compliance.

Unlike small consumer scales, industrial weighing systems are designed to handle heavier loads, harsher environments and continuous operation. Understanding how these scales work - and how to choose the right type - is essential for engineers, maintenance teams and procurement specialists responsible for production equipment.

This guide explains how weighing scales work, the most common types used in industry and the key factors to consider when selecting a weighing scale for industrial applications.

What are industrial weighing scales?

A weighing scale is a device used to measure the force exerted by an object due to gravity and convert that force into a readable weight value. Modern industrial scales typically rely on electronic sensors that convert mechanical force into electrical signals, which can then be processed and displayed as weight.

Industrial scales are designed for tasks such as:

  • Weighing raw materials during manufacturing
  • Checking product weights in packaging lines
  • Measuring pallets or bulk goods in warehouses
  • Monitoring material flow in processing plants

Because weight measurements often affect production quality, billing or regulatory compliance, industrial weighing equipment must be both accurate and reliable.

How industrial weighing scales work

Most modern weighing scales rely on load cells, which are sensors designed to measure force.

Inside a load cell are strain gauges attached to a metal element. When weight is applied to the scale, the metal element deforms slightly. This deformation changes the electrical resistance of the strain gauge, producing a small electrical signal proportional to the applied weight.

The process typically works like this:

  1. Force is applied – an object is placed on the scale platform.
  2. Load cells deform slightly under the applied weight.
  3. Strain gauges detect the change in resistance caused by this deformation.
  4. Electronics amplify the signal and convert it into a digital value.
  5. The weight is displayed or transmitted to a control system.

Depending on the size of the scale, there may be one or multiple load cells supporting the platform to ensure weight is distributed evenly and measured accurately.

This same principle is used in scales ranging from small bench units to large industrial weighbridges.

Set of scales in a warehouse

Common types of industrial weighing scales

Different industries require different industrial weighing scales depending on load size, required accuracy and how the weighing process fits into the wider workflow. Below are four common categories used across industrial, commercial and technical environments.

Hanging Scales

Hanging scales (sometimes called crane or hook scales) are designed to measure the weight of suspended loads. The scale is typically attached to a lifting mechanism such as a crane, hoist or hook, allowing the load to hang freely while its weight is measured.

These scales are widely used in industries where materials must be lifted during handling or processing.

Typical applications include:

  • Steel and metal fabrication
  • Construction materials handling
  • Warehousing and logistics
  • Agricultural produce weighing

Hanging scales are particularly useful when items are difficult to place on a platform or when weighing needs to occur during lifting operations.

View range

Platform Scales

Platform scales are among the most widely used industrial weighing scales, providing a flat surface where items can be placed for accurate measurement.

They are commonly used to weigh larger items such as pallets, containers or bulk goods, making them well suited to warehouse and manufacturing environments.

Typical uses include:

  • Pallet weighing in logistics operations
  • Incoming and outgoing goods checks
  • Manufacturing and packaging processes
  • Industrial shipping and dispatch

Depending on the model, platform scales can support loads ranging from tens of kilograms up to several tonnes.

View range

Pocket & Portable Scales

Pocket and portable scales are compact weighing devices designed for mobility and quick measurements. Their small size allows them to be easily carried between workstations, warehouses or field locations.

Despite their size, these scales can provide reliable measurements for lighter loads and smaller components.

Common uses include:

  • Quick product checks in warehouses
  • Jewellery and precious material weighing
  • Field inspections or mobile testing
  • Small parts measurement in workshops

Because they are lightweight and easy to transport, portable scales are particularly useful where weighing tasks need to be performed in multiple locations.

View range

Precision Scales

Precision scales are designed for applications that require high measurement accuracy and fine resolution.

These scales are commonly used where even small measurement variations can affect product quality or process outcomes.

Typical applications include:

  • Laboratory work and research environments
  • Electronics manufacturing
  • Pharmaceutical preparation
  • Quality control and testing

Precision scales generally offer higher resolution than standard industrial scales, allowing them to measure very small weight changes accurately.

View range

If you’re unsure which brand to choose, Kern is a strong place to start. With one of the most comprehensive and trusted weighing ranges on the market, they provide reliable, precision-engineered solutions suited to laboratories, production environments, quality control and wider industrial applications.

Kern banner

Industrial applications for weighing scales

Industrial weighing equipment supports a wide range of processes across many sectors.

Manufacturing

In manufacturing environments, weighing scales are used for:

  • Batching raw materials
  • Verifying component weights
  • Process control and quality assurance

Accurate measurements help ensure products meet specification and reduce material waste.

Logistics and warehousing

Logistics operations rely heavily on weighing scales to measure shipping loads and verify freight weights.

Typical uses include:

  • Pallet weighing
  • Parcel weighing
  • Freight compliance

Weight data can also be integrated into warehouse management systems.

Food and beverage production

Food processing operations use industrial scales to measure ingredients, control portion sizes and maintain consistent product quality.

Strict weight control is also necessary for regulatory compliance and packaging accuracy.

Chemical and pharmaceutical processing

In chemical manufacturing, precise weighing ensures that mixtures contain the correct proportions of raw materials.

Small measurement errors can affect chemical reactions or product quality, making reliable weighing systems essential.


Accuracy, capacity and resolution explained

When selecting a weighing scale, three specifications are particularly important.

1. Capacity

+

Capacity refers to the maximum weight the scale can measure safely.

Industrial scales may range from small bench units measuring a few kilograms to large truck scales capable of weighing tens of tonnes.

2. Resolution

+

Resolution describes the smallest weight change the scale can display.

For example:

  • A scale with 0.1 kg resolution will change readings in 100-gram increments.

Higher resolution is useful when measuring smaller items or when precise weight control is required.

3. Accuracy

+

Accuracy describes how closely the measured value matches the true weight.

Modern strain-gauge load cells commonly used in industrial scales can achieve accuracies within approximately 0.03% to 0.25% of full scale, depending on design and application.

However, scale accuracy can also be influenced by factors such as installation quality and environmental conditions.


Environmental factors that affect scale performance

Industrial environments can present challenges for weighing equipment.

Common factors that can affect scale accuracy include:

  • Vibration from nearby machinery
  • Uneven floors or mounting surfaces
  • Airflow from fans or ventilation systems
  • Temperature fluctuations
  • Moisture or dust contamination

For this reason, many industrial scales include protective housings and robust mounting systems to maintain measurement stability.

Calibration and maintenance

To maintain accuracy, industrial weighing scales must be calibrated periodically.

Over time, load cells can experience wear or slight mechanical shifts that affect measurement accuracy. Regular recalibration helps ensure reliable readings and many manufacturers recommend recalibration approximately once per year, depending on usage conditions.

Routine maintenance may also include:

  • Checking platform alignment
  • Verifying load cell operation
  • Inspecting cables and connectors
  • Cleaning debris from the weighing platform

Preventive maintenance helps extend the lifespan of industrial weighing equipment.

Choosing the right industrial weighing scale

Selecting the right weighing scale depends on several factors.

Load capacity

Choose a scale rated for the maximum expected weight, ideally with some margin for safety.

Required accuracy

Applications such as batching or pharmaceutical production may require higher precision than simple pallet weighing.

Installation environment

Consider whether the scale will be used in dusty, wet or high-vibration environments.

Integration requirements

Many industrial scales can connect to PLCs, production software or inventory systems to automate data collection.

Platform size

The weighing surface must be large enough to accommodate the objects being measured.

By considering these factors, organisations can select scales that deliver accurate measurements while supporting efficient production processes.

Upgrade your weighing

Although they may appear simple, industrial weighing scales are highly engineered systems that combine mechanical structures, precision sensors and electronic signal processing.

By converting force into electrical signals using load cells, modern scales can provide reliable weight measurements for applications ranging from small component counting to large-scale bulk material handling.

Whether used in manufacturing, logistics, food processing or chemical production, accurate weighing remains essential for quality control, safety and operational efficiency across modern industry.

Scales and balances banner
Share

Post a Comment



Trustpilot