Using heavy duty enclosures in harsh environments

Published on 17 June 26

Heavy duty enclosures are designed to protect critical electrical and electronic components in some of the most challenging operating conditions. From offshore installations to dusty manufacturing plants, these enclosures play a vital role in ensuring system reliability, safety, and longevity.

In this guide, we explore how heavy duty enclosures are used across harsh environments, and the key design considerations engineers and procurement teams must account for.

Why harsh environments require heavy duty enclosures

Standard enclosures often fall short in extreme conditions. Heavy duty enclosures are specifically engineered to provide:

  • High ingress protection (IP) against dust and water
  • Impact and corrosion resistance
  • Thermal stability in wide temperature ranges
  • Long-term durability in demanding environments

These features are essential for preventing equipment failure, reducing maintenance and ensuring safe system operation.

Offshore, marine and outdoor applications

Heavy duty enclosures are widely used in offshore platforms, marine systems and outdoor installations, where exposure to environmental elements is constant.

Key challenges:

  • Saltwater corrosion
  • Heavy rain and water ingress
  • UV radiation from sunlight
  • Wind, vibration and physical impact

Recommended solutions:

  • Stainless steel enclosures (316 grade) for superior corrosion resistance
  • IP66 or IP67 ratings for protection against powerful water jets and immersion
  • UV-resistant coatings for outdoor longevity
  • Sealed cable entry systems to maintain enclosure integrity

Typical applications:

  • Offshore oil & gas platforms
  • Coastal telecom infrastructure
  • Outdoor control panels
  • Renewable energy systems (solar, wind)

Protection against chemical exposure

In industries such as manufacturing, pharmaceuticals and chemical processing, enclosures must withstand exposure to corrosive substances and cleaning agents.

Common risks:

  • Chemical splashes or vapours
  • Cleaning processes using harsh detergents
  • Long-term material degradation

Best practices:

  • Use chemical-resistant materials such as stainless steel or specialised polymers
  • Avoid painted mild steel unless properly treated
  • Ensure seals and gaskets are compatible with chemical exposure

Application examples:

  • Food processing plants
  • Pharmaceutical production lines
  • Chemical handling facilities
  • Industrial washdown environments

Choosing the right enclosure material is critical in preventing corrosion-related failures and ensuring compliance with hygiene and safety standards.

Extreme temperatures

Heavy duty enclosures are frequently deployed in environments with very high or very low temperatures, where standard components may struggle to perform.

High-temperature environments:

  • Industrial furnaces
  • Foundries
  • Machine-heavy production facilities

Low-temperature environments:

  • Cold storage warehouses
  • Outdoor winter installations
  • Refrigeration systems

Key considerations:

  • Material expansion and contraction
  • Internal heat buildup from components
  • Reduced efficiency of electronics

Recommended solutions:

  • Thermally stable enclosure materials
  • Inclusion of cooling systems (fans, vents, heat exchangers)
  • Use of heaters in low-temperature environments to prevent condensation
  • Checking PSU and component derating curves

Proper thermal management ensures both the enclosure and its internal components maintain optimal performance.

High-dust and particulate environments

Industries such as construction, woodworking, and mining generate large amounts of dust and airborne particles, which can be highly damaging to electrical systems.

Risks:

  • Dust ingress causing short circuits or overheating
  • Reduced cooling efficiency
  • Increased maintenance requirements

Enclosure requirements:

  • High IP ratings (typically IP65 or above)
  • Dust-tight seals and gaskets
  • Filtered ventilation where airflow is necessary
  • Smooth surfaces for easy cleaning

Typical use cases:

  • Cement plants
  • Saw mills
  • Mining operations
  • Industrial workshops

Ensuring proper sealing and filtration prevents contaminants from compromising system performance.

Key design considerations across all harsh environments

Regardless of the specific application, several core factors should always be considered:

Material selection

  • Stainless steel for corrosion resistance
  • Mild steel for cost-effective indoor use
  • Polycarbonate for lightweight, corrosion-proof solutions

Ingress protection (IP Rating)

  • Match rating to environment (dust, moisture, washdown)

Sealing & gasketing

  • Ensure long-term durability under exposure conditions

Ventilation & cooling

  • Prevent overheating without compromising protection

Mounting & accessibility

  • Ensure ease of installation and maintenance

Why proper enclosure selection matters

Using the wrong enclosure in a harsh environment can lead to:

  • Equipment failure
  • Increased downtime
  • Safety risks
  • Higher maintenance costs

By selecting a heavy duty enclosure tailored to the operating environment, businesses can improve system reliability and reduce long-term operational costs.

Conclusion

Heavy duty enclosures are essential for protecting electrical systems in harsh environments, from offshore and outdoor installations to chemically aggressive and high-dust settings. By considering factors such as material, IP rating, temperature resilience, and environmental exposure, engineers can ensure their systems remain safe, reliable, and efficient.

Investing in the right enclosure is not just about protection—it’s about maintaining performance in the environments that demand it most.

Popular heavy duty enclosures

Share

Post a Comment



Trustpilot