Flow sensors in modern control systems

Published on 13 January 26

Flow sensors are essential components for monitoring, controlling and safeguarding fluid and gas systems. From industrial process lines to HVAC systems, automotive engines and medical devices, they provide real-time insight into volume, velocity or mass flow, enabling efficient operation and safety compliance.

Flow sensor selection

Selecting the right flow sensor involves more than matching flow range - engineers and buyers must consider sensor type, media compatibility, accuracy, response time and environmental suitability. This guide helps you evaluate, compare and confidently select flow sensors for your application.

How flow sensors work

Flow sensors convert the movement of a fluid or gas into an electrical signal. They differ widely in operating principle, accuracy and application suitability:

  • Volumetric flow sensors measure the volume of fluid per unit time (litres/min, gallons/min).
  • Mass flow sensors measure the mass passing through a system (kg/h, lb/min), accounting for density and temperature changes.
  • Flow switches provide on/off detection rather than continuous measurement.

How do thermal flow sensors work in HVAC systems?

Thermal flow sensors operate on the principle that the rate of heat transfer from a heated surface to a moving fluid is directly proportional to the fluid's mass flow rate. In HVAC systems, these sensors typically utilise a pair of precision thermistors or resistance temperature detectors (RTDs). One element measures the ambient air temperature as a reference, while the second is actively heated to maintain a specific temperature differential above that ambient level.

Common measurement principles

  • Thermal (hot-wire or thermistor-based): Measures airflow or gas flow by detecting heat dissipation. Highly sensitive for low flow rates, often used in HVAC or medical devices.
  • Turbine or paddle wheel: Uses a rotating element whose speed is proportional to flow. Suited to liquids or clean gases; moderate accuracy, simple installation.
  • Differential pressure / Venturi / Orifice: Measures flow by detecting pressure drop across a constriction. Robust, widely used in industrial processes.
  • Ultrasonic: Uses sound waves to measure flow velocity without contacting the fluid; excellent for clean or corrosive liquids.
  • Electromagnetic: For conductive liquids, measures flow based on voltage induced in a magnetic field; high accuracy, suitable for water and chemical process control.

Flow sensors are integral components of several modern automated control architectures

  • Industrial Control Systems (ICS): Flow data is a primary input for Programmable Logic Controllers (PLCs) used for discrete machine control, Distributed Control Systems (DCS) for complex plant-wide processes like oil refining and Supervisory Control and Data Acquisition (SCADA) systems for monitoring geographically dispersed assets like pipelines and electrical grids.
  • Building Automation and Management Systems (BAS/BMS): These systems use flow sensors to manage Variable Air Volume (VAV) boxes and airflow measuring stations, optimising ventilation rates, building pressurisation and energy efficiency.
  • Smart Water and Environmental Networks: Modern utility management utilises IoT-enabled water management systems and Digital Twins (virtual replicas of physical networks) to monitor real-time flow, predict demand and detect leaks using AI-driven algorithms.
  • Enterprise Automation Platforms: Leading industrial suites integrate flow sensor data into cloud-based analytics for predictive maintenance and facility-wide optimisation.
  • Automated Dosing and Treatment Systems: In wastewater and chemical processing, specialised systems from providers use flow feedback to automate precise chemical dosing for pH balancing and disinfection.

Airflow sensors

Airflow sensors are a subset of flow sensors designed to measure air or gas velocity. They are commonly used in:

  • HVAC systems for duct monitoring
  • Industrial ventilation
  • Engine management systems (MAF sensors in automotive)
  • Environmental monitoring

Key considerations include response time, pressure drop and sensitivity to contaminants, since even small particles or moisture can affect measurement accuracy.

Airflow sensors for HVAC systems

Airflow sensors are critical for managing ventilation and building pressurization by providing real-time feedback to automation systems. These sensors typically employ thermal dispersion technology to measure mass flow through heat dissipation, maintaining high sensitivity even at extremely low velocities where mechanical alternatives often fail. In Variable Air Volume (VAV) systems, they facilitate precise damper modulation and support energy-saving logic.

How do mass airflow sensors work in automotive applications?

Automotive mass airflow (MAF) sensors utilize a "hot wire" or "hot film" element heated to a fixed temperature above ambient air to measure intake mass via thermal dispersion . As incoming air cools the element, a control circuit increases the electrical current to maintain the set temperature differential. This current is directly proportional to the air mass and is transmitted to the Engine Control Unit (ECU) to determine the ideal fuel-to-air ratio for efficient combustion.

Flow meters vs flow switches

Flow meters provide continuous measurement and are selected when precise volume or mass tracking is required.

Flow switches trigger an action when flow exceeds or drops below a threshold, often used for pump protection, safety interlocks or system alarms.

Choosing between them depends on control objectives and required data granularity.

Selection considerations

1. Media compatibility

  • Fluid type: water, oil, fuel, chemicals
  • Gas type: air, compressed gases, exhaust

Why it matters: Media incompatibility can cause corrosion, swelling or sensor degradation, leading to inaccurate readings or premature failure.

2. Temperature and viscosity

  • Corrosion and chemical resistance of sensor materials

Selecting an incompatible sensor can lead to rapid failure, measurement drift or safety hazards.

3. Accuracy & repeatability

  • Specify accuracy based on process or regulatory requirements
  • Consider linearity across flow range
  • Review calibration drift and maintenance requirements

High-accuracy sensors may require periodic recalibration; lower-cost options may be suitable for non-critical monitoring.

4. Pressure drop & flow impact

  • Flow sensors inevitably impose some resistance on the system
  • Minimise pressure drop in sensitive systems (compressed air, HVAC ducts, fuel lines)
  • Check manufacturer-specified ΔP for your expected flow rates

What is the difference between volumetric and mass flow measurement?

Volumetric flow measures the space fluid occupies as it moves (ex: liters per minute), which can change if the fluid expands or contracts. Mass flow measures the actual number of molecules. Mass flow sensors are superior for gases and critical chemical processes because they provide consistent data regardless of fluctuations in temperature or system pressure.

Environmental & installation factors

  • Mounting orientation can affect turbine or thermal sensors
  • IP rating and protection against dust, moisture or chemicals
  • Temperature and vibration tolerance
  • Power supply, output type and signal interface compatibility

Procurement & lifecycle considerations

  • Standardisation: Prefer sensors with documented specifications and multiple qualified suppliers
  • Maintenance: Consider ease of cleaning, replacement and calibration
  • Integration: Ensure compatibility with existing controllers, PLCs or data acquisition systems
  • Long-term availability: Industrial projects often outlast sensor lifecycles; selecting widely adopted models reduces replacement risk

Compliance & standards notes

Depending on the application, flow sensors may need to meet:

  • ISO 9001 / ISO 4064 for water flow
  • CE, UL or CSA for electrical safety
  • FDA or medical device standards for biomedical applications
  • Environmental directives like RoHS and REACH

Summary

Flow sensors are more than simple measurement devices; they are critical enablers of process control, safety and efficiency. Selecting the right sensor requires evaluating sensor type, media compatibility, accuracy, response time, environmental factors and long-term supply reliability. By combining careful technical evaluation with supplier verification, engineers and procurement teams can ensure the chosen flow sensor provides reliable performance throughout the system lifecycle.

Browse flow sensors Browse all sensors

FAQs

What is a flow sensor used for?

+

Flow sensors measure the movement of liquids or gases and provide feedback for control, monitoring or safety purposes.

What is the difference between a flow meter and a flow switch?

+

A flow meter provides continuous measurement; a flow switch triggers an action when flow exceeds or drops below a threshold.

Can a flow sensor measure both liquid and gas?

+

Most sensors are designed for a specific medium; select based on fluid type, viscosity and temperature.

What is an airflow sensor?

+

An airflow sensor measures the velocity or volume of air in a duct, engine intake or gas system, often using thermal or turbine principles.

How do I choose between different flow sensor types?

+

Consider media compatibility, accuracy, pressure drop, installation environment and maintenance requirements. Match sensor principles to application needs.

Share

Post a Comment



Trustpilot