Discover the Dobot CR5

Published on 02 October 25
Dobot robotic arms on an assembly line

Dobot is at the forefront of robotic innovation, developing flexible, intelligent robotic arms for both industrial automation and advanced research. The Dobot CR5 is a prime example, combining precision, versatility, and user-friendly programming to empower everyone from engineers to students. Compact yet powerful, it delivers reliable performance whether on the factory floor or in a robotics lab. This article explores the CR5’s key features, applications, and real-world benefits, showing why it’s a standout choice for both industrial and educational environments.

Why choose Dobot?

What makes Dobot unique is its focus on turning advanced robotics into practical, everyday solutions. Its collaborative robots are designed with safety, scalability, and adaptability at their core, enabling seamless integration into diverse workflows. With intuitive interfaces and a growing ecosystem of plug-and-play accessories, Dobot ensures users can innovate without compromise.

For businesses, this means safer operations, reduced downtime, and measurable productivity gains; for educators, it means accessible, future-ready tools that inspire the next generation of problem-solvers. Trusted by organisations worldwide, Dobot continues to redefine how robotics drive progress across industries and education.


Product overview

The Dobot CR5 is built to combine precision and accessibility, making it a powerful yet approachable choice for both industrial users and researchers. Compact, versatile and easy to operate, it’s designed to streamline workflows without unnecessary complexity.

Introducing the Dobot CR5 Collaborative Robot

Josh, our technical product specialist, provides an in-depth look at the CR5 in action, showcasing its 5kg payload and 900mm reach as it carries out tasks such as pick-and-place, stacking and even drawing. Beyond its technical strength, the CR5 demonstrates how user-friendly robotics can be, with drag-to-teach programming and the intuitive DobotStudio interface. Its compact control cabinet keeps workspaces organised, reinforcing its practical design. Whether used on production lines or in research projects, the CR5 stands out for its adaptability and consistent performance.

The consistency of the 6-axis architecture and core mechanical specifications across the entire CR5 series is a key differentiator. The stable mechanical foundation guarantees that the fundamental precision and accuracy of task execution remain constant, irrespective of the specific model chosen by the end-user.

Features & benefits

The CR5 doesn’t just deliver specifications on paper, it offers real advantages that simplify installation, enhance usability, and scale to different environments. From reducing downtime to encouraging innovation, it’s engineered to support both industry and academia.

Advanced safety and collaboration features

Safety is integral to the CR5 design, allowing the arm to work safely alongside human operators:

  • Safety Baseline: All models include essential safety mechanisms such as electromagnetic brakes and a system for real-time payload detection.
  • SafeSkin Technology (S-variants): Certain variants feature SafeSkin, a contactless pre-collision safety system that utilizes electromagnetic field sensing to detect approaching objects without relying on vision sensors.
  • Optimised Collision Avoidance: SafeSkin provides 360-degree obstacle detection over the entire front portion of the arm. It can detect objects within a 15cm range and initiate a response in just 0.1 seconds, significantly minimizing the potential for collision impact.

Why choose the Dobot CR5?

Josh highlights why the CR5 is more than just another collaborative robot. He explains its industrial-grade performance paired with academic flexibility, ensures it can serve as both a production tool and a teaching platform. Its streamlined control cabinet makes installation straightforward, while plug-and-play accessories expand its functionality for more advanced applications. By showcasing its intuitive interface, quick task setup and scalability, the CR5 positions itself as a cost-effective yet innovative solution that grows with your needs, whether in smart factories or educational settings.

Functionality in industrial & research applications

The strength of the CR5 lies in its ability to transition seamlessly between environments. It’s engineered to perform in demanding industrial settings while remaining flexible enough for experimental and educational use.

Real-world use cases for the CR5

Josh demonstrates how the CR5 fits into real-world scenarios with ease. In industry, it delivers high-precision, repetitive task performance, excelling at inspection, sorting and light assembly while reducing errors and improving efficiency. In research and education, it enables practical learning and experimentation across automation, AI, and human-robot interaction. With modular design, broad I/O support and open programming options, the CR5 adapts from prototype testing to production-ready systems. This flexibility ensures it delivers tangible value across a wide range of applications, making it a reliable choice for engineers, educators and innovators.


Next steps

Discover how the Dobot CR5 can transform your workflow, whether on the factory floor or in the classroom. Contact our team today to explore its capabilities and see how it can meet your automation or research needs.

Share

Post a Comment



Trustpilot