Cable management for industrial panels: clips, trunking & sleeving

Published on 22 April 26

Cable management inside industrial panels is about far more than keeping things tidy. Done properly, it improves safety, simplifies maintenance, reduces downtime and helps ensure long-term reliability. Done poorly, it can lead to overheating, electrical interference, difficult fault finding and costly rework.

This guide breaks down the most effective cable management methods - clips, trunking and sleeving - and explains how to apply them in real-world panel builds.

What good cable management looks like

In a well-designed industrial panel, cable management should achieve four key things:

  • Clear organisation – cables are easy to trace and identify
  • Safe separation – power and signal cables are routed appropriately
  • Efficient airflow – wiring does not restrict cooling
  • Maintenance access – technicians can work without disruption

By contrast, poor cable management often results in overcrowded wiring, unclear routing and limited accessibility, issues that typically only become apparent during maintenance or fault finding.

Cable management methods explained

The three methods used most often in panel builds are cable clips, trunking and sleeving. Here’s how each works and where it fits.

Cable clips

Cable clips are one of the simplest ways to securely hold and neatly route cables within a panel or enclosure.

Key advantages

  • Quick and easy to install
  • Flexible positioning
  • Ideal for small-scale or retrofit work

Limitations

  • Less structured than trunking
  • Can become disorganised in high-density panels

In practice, cable clips are often used where flexibility is needed, such as adding or rerouting cables after installation.

Trunking (cable duct)

Trunking is the most widely used solution for structured cable management in control panels. It provides a defined pathway for routing and organising cables.

Key advantages

  • High level of organisation
  • Keeps wiring contained and protected
  • Makes future modifications easier

Types

  • Slotted trunking – allows cables to exit at multiple points
  • Solid trunking – offers greater protection but less flexibility

In most panel builds, trunking forms the backbone of the cable management system, especially where cable density is high.

Cable sleeving and conduit

Sleeving and conduit are primarily used for protecting and bundling cables rather than structuring them within the panel.

Key advantages

  • Protects against abrasion and wear
  • Helps group cables together
  • Useful for cables entering or exiting the panel

Limitations

  • Doesn’t provide the same level of organisation as trunking
  • Can make individual cables harder to access

Sleeving is typically used alongside other methods rather than as a standalone solution.

How do cable sleeving and conduit protect industrial wiring?

While trunking organises cables, cable sleeving and conduit are primarily used for mechanical protection and bundling. Sleeving protects individual wires or small groups from abrasion, chemicals and heat, especially where cables transition between the panel body and moving parts like doors. Conduit provides the highest level of environmental protection, acting as a rigid or flexible barrier against moisture and physical impact.

Side-by-side comparison

Performance comparison: clips, trunking and sleeving
Feature Cable clips Trunking Sleeving
Flexibility High Medium High
Organisation Low High Medium
Protection Low Medium High
Best use Small or retrofit jobs Structured panel wiring Protection and bundling

When should you use cable trunking versus cable clips?

The choice between cable management methods depends on the density of the wiring and the need for future flexibility. Trunking (cable duct) is the industry standard for high-density, structured panel builds, providing a protected pathway for large bundles of wire. Cable clips, conversely, offer high flexibility for small-scale projects or retrofitting additional wires where installing a full duct system would be impractical.

How to choose the right approach

The best cable management strategy depends on your application.

For new control panel builds

Use trunking as the primary method. It provides structure, scalability and easier long-term maintenance.

For retrofits or modifications

Use a combination of cable clips and existing routing, allowing flexibility without major redesign.

For cables requiring protection

Add sleeving or conduit, particularly where cables are exposed to movement or abrasion.

In many real-world panels, a hybrid approach is used - trunking for structure, clips for flexibility, and sleeving for protection.

Cable routing best practices

This is where cable management moves from “tidy” to truly effective.

Separate power and signal cables

Routing high-power and low-voltage signal cables together can introduce electrical interference. A common issue in panel builds is signal noise caused by poor separation - something that’s easy to avoid with proper planning.

Maintain service loops

Leaving a small amount of slack in cables reduces strain on connections and makes maintenance and replacement easier. Overly tight wiring might look neat initially, but it often creates problems later.

What is a “service loop” and why is it essential in cable routing?

A service loop is a deliberate amount of slack left in a cable run, usually near the termination point. This prevents mechanical strain on connectors, which can cause loose connections over time. More importantly, service loops provide the length technicians need to re-terminate a wire or move a component during maintenance without having to rewire the entire panel.

Avoid overfilling trunking

Packing too many cables into trunking restricts airflow, makes modifications difficult and increases the risk of overheating. In practice, allowing spare capacity is one of the simplest ways to future-proof a panel.

Plan cable entry and exit points

Well-planned routing paths reduce clutter, improve organisation and make installations more consistent.

Heat, airflow and panel performance

Cable management directly affects thermal performance. Dense or poorly routed wiring can block airflow, trap heat and reduce component lifespan.

A common misconception is that tighter cable routing is always better. In reality, allowing space for airflow is just as important as organisation.

Why is cable management critical for industrial panel reliability?

Effective cable management is an engineering necessity that supports safety, airflow and electromagnetic compatibility (EMC). Beyond organisation, properly managed cables prevent signal noise by separating power and data lines, reduce thermal stress by maintaining clear airflow paths for components, and significantly lower mean time to repair (MTTR) by allowing technicians to trace and identify circuits quickly.

Maintenance and future-proofing

Good cable management doesn’t stop at installation - it should support the entire lifecycle of the panel.

Key considerations

  • Clear labelling for quick identification
  • Spare capacity for future additions
  • Accessible routing for fault finding

In many maintenance scenarios, the difference between a 10-minute fix and a 2-hour job comes down to how well the cables were managed initially.

Common mistakes to avoid

Even experienced installers can run into issues. Some of the most common include:

  • Overcrowding trunking
  • Mixing power and signal cables
  • Leaving no slack in wiring
  • Poor or inconsistent labelling
  • Using the wrong method for the application

Compliance and safety considerations

Cable management also plays a role in meeting safety and regulatory requirements. Key factors include:

  • Appropriate separation of circuits
  • Use of materials with suitable fire performance
  • Adequate insulation and protection

While requirements vary by application, good cable management practices naturally support safer, more compliant installations.

What to look for when choosing cable management products

When comparing cable management products, look for:

  • Build quality and durability
  • Temperature resistance
  • Ease of installation
  • Compatibility with your panel layout
  • Availability of accessories (covers, dividers and so on)

Final thoughts

Effective cable management in industrial panels is about more than appearance - it directly impacts performance, safety and ease of maintenance.

By combining structured solutions like trunking with flexible options such as clips and protective sleeving, you can create installations that are not only neat, but practical and future-ready.

Ultimately, a well-managed panel is easier to work on, easier to expand and far more reliable over the long term - and that’s where the real value lies.

Ready to organise your next build?

Explore our full range of cable clips, trunking and sleeving solutions to get the job done right.

Share

Post a Comment



Trustpilot