A breadboard lets you build and change circuits without soldering, by pushing component legs into a grid of holes. The one thing that makes it click: the holes are not independent — they're joined underneath by hidden metal strips. Short strips run across the board in rows of five for your components, and long strips run down the sides as power rails. Picture those strips and the breadboard stops being a mysterious grid.
Almost every beginner mistake — parts that look connected but aren't, accidental shorts, power not reaching where you expect — comes from not seeing the strips. Get that mental model and the rest is straightforward.
Breadboards are where most people build their first circuit, which makes them the backbone of electronics teaching and hobby prototyping alike. This guide explains what's happening underneath the surface, how to place components and power correctly, and where a breadboard's limits are. If you're working from a schematic, our guide to circuit symbols covers reading the diagram you'll be building from.
How is a breadboard connected inside?
A standard breadboard has a large central block of holes divided by a channel down the middle, with long rails running down each outer edge. Those are three different connection patterns, and knowing them is the whole game. In the central block, holes are joined in short vertical columns of five — each column of five is one electrical point, so anything plugged into it is connected. The columns are not joined to each other, and not joined across the central channel. That channel is deliberate: it splits each row into two halves so you can straddle a chip (a DIP integrated circuit) across the gap, with its two rows of legs landing in separate, unconnected columns. The long rails down the edges are the power buses; they run the length of the board for your positive supply and ground, so any component can reach power with a short jumper. One common trap: on some boards the side rails are split into two halves rather than running unbroken end to end, so if power seems to stop halfway, a short jumper across the break restores it.
How do you build a circuit on a breadboard?
Start by wiring your power rails: run a jumper from the supply's positive terminal to a red rail, and from ground to a blue or black rail. Feeding both sides from the start saves rewiring later. Then place components so the legs you want connected share a column, and the legs you want separate sit in different columns or across the central channel. Jumper wires bridge everything else — column to column, or column to power rail. Building tidily, with wires kept short and flat, isn't just neatness: a rat's nest is almost impossible to fault-find, whereas a flat, logical layout lets you trace the circuit by eye. Because nothing is soldered, you can pull a component and reposition it as often as you like, which is exactly what makes breadboards so well suited to classroom experimentation and quick prototyping.
What are the most common breadboard mistakes?
Nearly all of them trace back to the hidden strips. These are the ones that catch people out most often.
| Symptom |
Usual cause |
Fix |
| Two parts won't connect |
Their legs are in the same row but opposite sides of the central channel |
Put both legs in the same column, or bridge with a jumper |
| Circuit dead at one end |
Split power rail — the rail breaks in the middle |
Add a jumper across the break to join the two halves |
| Intermittent connections |
Component legs too thick, or a worn board |
Use solid-core wire; retire boards with loose contacts |
| Accidental short circuit |
A stray leg or wire bridging two columns that shouldn't meet |
Trim long legs; check nothing crosses the channel unintentionally |
When should you stop using a breadboard?
A breadboard is a prototyping tool, not a permanent home for a circuit. The spring contacts add resistance and stray capacitance, so breadboards are poor for high-current, high-frequency and sensitive analogue work, and the push-fit connections work loose with handling — so a circuit you want to keep or carry should be moved on. The usual next step is stripboard or a custom PCB, where connections are soldered and permanent. If your circuit uses fiddly surface-mount chips or sensors, a breakout board bridges the two worlds; our guide to breakout boards explains how those make awkward components breadboard-friendly. When you're ready to build for keeps, the wider prototyping and PCB development range covers the move to a permanent board.
Getting started or restocking the classroom? Browse our range of solderless breadboards and jumper wires.
Browse breadboards
Common questions
Which holes on a breadboard are connected?
In the central area, holes are joined in short columns of five, and the two halves are separated by the central channel. The long rails down each edge are connected along their length as power and ground buses, though some boards split these in the middle.
Why is there a gap down the middle of a breadboard?
The central channel separates the two halves of each row so you can straddle a DIP integrated circuit across it. Each row of the chip's legs then lands in its own set of unconnected columns, giving every pin an independent connection point.
Do you need to solder anything on a breadboard?
No — that's the point of a breadboard. Components and wires push into the holes and grip against internal spring contacts, so circuits can be built and changed freely. This makes breadboards ideal for learning and prototyping before committing to a soldered board.
What can't you use a breadboard for?
Breadboards suit low-power prototyping. They're poor for high-current, high-frequency or sensitive analogue circuits because the spring contacts add resistance and stray capacitance, and the push-fit connections loosen with handling. Permanent or portable circuits should move to stripboard or a PCB.