Genie 13-6026 Serial LCD Kit

MPN
13-6026
Brand
Genie
Order Code
13-6026
Country of Origin
Thailand
  • Free UK shipping available
  • Quickly find another product in this range by Type:

    LCD Control chip Serial LCD kit
View Full Product Range (2)
Qty Unit Price (Ex VAT)
1+ £20.04
Price per unit {{ this._page.IncVat ? 'Inc' : 'Ex' }} VAT
Despatched same day - 28 in stockAdditional quantity lead time 3 weeks

The GENIE Serial LCD module allows GENIE-based projects to display messages on a LCD. The kit includes full instructions on how to construct the LCD module and then explains how to connect to GENIE microcontrollers in order to output text and graphics.



  • 16 character by 2 row liquid crystal display (LCD)
  • Contrast dial for display
  • All components included in kit
  • A spare LCD control chip (13-6036) is also available separately
  • Testing mode included

Full and comprehensive instructions can be obtained here

The GENIE Design Studio software is free to download directly from www.genieonline.com.


Type Serial LCD kit

Questions

*Question functionality currently disabled
Question by: Product code: 13-6026

Q. What are the dimentions

A. Hi Theo, thank you for your question. The dimensions are as follows: 92mm length, 45mm width and 13mm height. Please see the data sheet.

Question by: Product code: 13-6026

Q. What connectors does this require - I see a 3 pin molex type connector for power and serial. What is the rapid code for these?

A. Hi Andrew, thank you for your question. The following headers could be used or they can be soldered directly to: 22-0840 3 way + 22-0822, 22-0838 2 way + 22-0820 and crimps 22-0836.

Question by: Product code: 13-6026

Q. Does the kit come with all the components needed for assembly

A. Hi Jake, thank you for your question. Yes this is a complete kit that will require assembly with a soldering iron and basic tools (not supplied).

Question by: Product code: 13-6026

Q. I have assembled the lcd module and fully checked everything is in placed. The screen does not show anything even on test mode. Any ideas what is wrong. Am I right to assume that the driver code is already loaded on the supplied PIC chip?

A. Hi John, thank you for your question. We would suggest trying the contrast control first (potentiometer on PCB) page 5 of the data sheet ensuring the power supply is accurately between 4.5-5.5V maximum and double check all the soldering connections made.

Question by: Product code: 13-6026

Q. Where do I put the battery as it has red and black wire. But in the instructions it doesn't say where they need to go.

A. Hi Ryan. Thank you for your question. The red wire goes to the positive (+) and the black wire goes to the negative (-).

Question by: Product code: 13-6026

Q. I am wondering if I could get a data sheet for the actual LCD used in this product, I would like to compare its PIN Function with other displays. many thanks

A. Hi Stephen. Thank you for your question. Please see the data sheet for the requested LCD.

Question by: Product code: 13-6026

Q. what are the dimensions of the whole product, including the PCB

A. Hi Sam. Thank you for your question. The dimensions are 92mm x 45mm x 15mm.

Question by: Product code: 13-6026

Q. What are the dimensions of the black border area around the screen?

A. Hi Adam. Thank you for your question. The black outer surround is 25mm x 73mm. The screen window is 16mm x 61mm within it.

Question by: Product code: 13-6026

Q. Can it be controlled via the control device option in circuit wizard?

A. No, the control device option will only set High or Low level not provide the more complex programming required for this unit.

Question by: Product code: 13-6026

Q. Is it possible to connect a Genie chip to any other backlit LCD display?

A. Thanks for your enquiry Bill. This particular module has been constructed so that the PCB backplate accepts the data lines in the correct order. There is no reason why another display could not be used but care must be used to ensure the display input lines are correctly connected to the appropriate pins.

Question by: Product code: 13-6026

Q. How big is the LCD screen itself, including the black plastic that surrounds it?

A. Hi Jack, thanks for your question. 57-0911 is the screen used, please see the data sheet link below for dimensions: https://www.rapidonline.com/pdf/57-0911.pdf

Question by: Product code: 13-6026

Q. I think i've lost the instructions sheet where it tells you where to put the components. So i don't know where to solder what yet. I am using this on my electronics project in y11 so please can you hel me?

A. Hi Jack, thanks for your question. Please refer to the datasheet for more information, this will help you with what you need https://www.rapidonline.com/pdf/13-6026.pdf

Question by: Product code: 13-6026

Q. What size is this product?

A. The unit is 83L x 44W x approx 14mm (assembled) (please note that the thickness is an estimate)

Question by: Product code: 13-6026

Q. can this be used on a co8 activity board?

A. Hi Alistair, thanks for your enquiry. Yes this module can be connected to the CO8 board. Select output 'G2' for the serial signal.

Reviews

Be the first to submit a review

Trustpilot