We use cookies on our website to ensure you get the best possible experience – they allow us to tailor content specifically to you, analyse our website to help make improvements, and display ads that are applicable to you across other websites. If you’re happy with this, please select “Allow all", or personalise the cookies you allow with “Manage”. Clicking on “Reject non-essential” will remove these cookies, but the site may not function to its best abilities. For more information, please visit our cookie policy
Polycarbonate vs steel enclosures: which should you choose?
Published on 12 February 26
In industrial and commercial environments, enclosures do far more than simply house components. They protect sensitive equipment, ensure electrical safety, maintain compliance and help extend the lifespan of critical systems.
When specifying an enclosure, material choice is one of the most important decisions. Two of the most widely used options are polycarbonate and steel - both offering excellent protection, but suited to very different environments.
So how do you decide which is right for your application?
Why enclosure material matters
The material of an enclosure directly affects:
Mechanical strength
Resistance to corrosion and chemicals
Electrical insulation
Installation requirements
Long-term durability
Overall project cost
Choosing the wrong material can lead to premature failure, unnecessary expense or compliance issues. Understanding the differences between polycarbonate and steel ensures the enclosure performs reliably in its intended environment.
For more clarification on which enclosure suits best, read our full user's guide here
Polycarbonate enclosures are widely used across automation, electrical control, telecommunications and general industrial installations. They're engineered plastics designed to offer strong impact resistance while remaining lightweight and electrically insulating.
Key advantages
1. Lightweight and easy to install
Polycarbonate enclosures are significantly lighter than metal alternatives. This simplifies handling, mounting and transportation - particularly in wall-mounted or pole-mounted applications.
2. Natural electrical insulation
As a non-conductive material, polycarbonate provides inherent electrical insulation. This reduces the need for additional grounding considerations and can simplify system design.
3. Corrosion resistance
Polycarbonate does not rust and performs well in damp or moderately corrosive environments. Many variants are also resistant to common industrial chemicals.
4. Cost-effective solution
In many applications, polycarbonate offers a lower upfront cost compared to steel, making it attractive for budget-sensitive projects or large-scale rollouts.
5. Strong ingress protection
High-quality polycarbonate enclosures are available with IP65, IP66 or higher ratings, providing excellent protection against dust and water ingress.
Considerations
Lower temperature tolerance compared to steel
Not ideal for extremely harsh mechanical environments
For control panels, automation systems and outdoor electrical installations, polycarbonate often delivers the right balance of durability, insulation and value.
Why is polycarbonate preferred for 5G and wireless connectivity?
In 2026, the rise of "Physical AI" and IoT means enclosures often house wireless transmitters. Steel and stainless steel act as a Faraday cage, blocking RF and Wi-Fi signals unless external antennas are installed. Polycarbonate is transparent to radio waves, allowing you to keep Wi-Fi routers, 5G gateways and Bluetooth sensors safely locked inside the box while maintaining full signal strength.
Steel enclosures: strong and economical
Steel enclosures are widely used in industrial and commercial settings where mechanical strength and cost-effectiveness are important. They are commonly specified in manufacturing, facilities management and electrical distribution systems.
Key advantages
1. Exceptional mechanical strength
Steel offers superior structural integrity, making it suitable for industrial environments with potential impact or heavy components.
2. Cost-effective durability
Plain steel is generally less expensive than stainless steel while still providing strong protection for indoor or covered environments.
3. Long service life (with protection)
When properly coated or painted, steel enclosures can withstand moderate environmental exposure and maintain structural integrity over time.
4. Suitable for larger installations
Steel is often preferred for large electrical cabinets, switchgear or control panels due to its strength and rigidity.
Considerations
Susceptible to rust in wet or outdoor environments without proper coating
Requires grounding due to electrical conductivity
Heavier and more challenging to install than polycarbonate
Modifications on site (cutting/drilling) are more labor-intensive
Steel enclosures are ideal for indoor industrial applications, dry environments or locations where mechanical strength and cost savings are priorities.
Comparing performance by application
Instead of asking which material is “better,” it’s more useful to consider the specific environments where polycarbonate enclosures and steel enclosures perform best.
Outdoor installations
Polycarbonate enclosures are naturally corrosion-resistant and UV-stabilised variants work well outdoors. Whereas, steel enclosures require protective coatings to prevent rust and are less suitable in exposed environments.
Washdown & hygienic environments
Polycarbonate has an advantage in moisture-rich areas. Plain steel can corrode if exposed to repeated washdowns or chemicals unless coated with corrosion-resistant paint.
Electrical safety
Polycarbonate provides inherent electrical insulation, reducing grounding needs. Steel is conductive and requires proper grounding in all installations.
Installation & handling
Polycarbonate is lighter and easier to install. Steel’s weight requires more careful planning and hardware for mounting.
Budget-conscious projects
Steel can provide a lower-cost solution for indoor or controlled environments, whereas polycarbonate may offer better overall value in corrosive or outdoor settings.
What are the electrical grounding and safety requirements for each?
Safety is the biggest logistical difference between these materials:
Steel Enclosures: Being conductive, steel requires a dedicated safety ground (earth) connection. If a live wire touches the metal casing, the ground path ensures a circuit breaker trips rather than energising the box and creating a shock hazard.
Polycarbonate Enclosures: As a natural insulator, polycarbonate is "double-insulated." It cannot become live, which simplifies wiring, reduces the risk of arc-flash incidents during maintenance, and eliminates the labour time required for grounding the enclosure itself.
Cost vs lifetime value
Steel enclosures are generally cheaper upfront, but in environments where corrosion is an issue, they may require repainting or additional protective measures. Polycarbonate, while sometimes slightly more expensive initially, often delivers a longer effective lifespan outdoors or in humid conditions.
Choosing the right material depends on:
Environmental exposure
Mechanical risk
Compliance requirements
Installation constraints
Expected lifespan
Which enclosure material is right for you?
As a general guide:
Choose polycarbonate if you need:
Lightweight construction
Strong electrical insulation
Natural corrosion resistance
Flexible installation options
Choose steel if you need:
High mechanical strength
Cost-effective indoor protection
Rigid structure for large or heavy cabinets
Controlled environment applications
Which material offers better thermal management for electronics?
Steel has high thermal conductivity. It can act as a giant "radiator," helping to pull heat from internal components and dissipate it into the cooler outside air.
Polycarbonate is an insulator; it holds heat inside. If your enclosure houses high-heat components (like VFDs or large power supplies) in a hot environment, you may need to add active ventilation (fans) or heat sinks to a polycarbonate box to prevent internal electronics from overheating.
Final thoughts
There is no universal “best” enclosure material - only the best fit for your application. Both polycarbonate and steel offer excellent protection when correctly specified.
By understanding the environmental demands, compliance needs and lifecycle expectations of your project, you can select an enclosure that ensures long-term performance, safety and reliability.