The Fluke BP120MH Battery Pack is the correct replacement battery for the Fluke 120 series ScopeMeters and in the Fluke 43 and 43B Power Quality Analyzers. The BP120MH is a Nickel-Metal-Hydride Battery Pack, made specifically to support the ScopeMeters and Power Quality Analyzers mentioned.
The battery capacity is 3000mAh, this is 50% more than that of the original BP120. As a results, the instrument-user will benefit from a much longer ‘up time' than with the original Ni-Cd battery, at the same volume and weight.
The Fluke BP120MH is more environmental-friendly than the Ni-Cd battery used before, as it contains no heavy metals. Just as before, the battery pack can be charged while installed in the instrument, using the PM8907 power adaptor/charger.
The BP120MH replaces the earlier models BP120 and BP130 alike.
- Nominal voltage: 4.8V
- Capacity: 3000mAh
- Manufacturers part no. Fluke BP120MH
To use this facility please Sign In.
Sign In