15 July 26
A metric fastener designation reads diameter × pitch × length: M6 × 1.0 × 20 is a 6 mm nominal diameter thread with a 1.0 mm pitch, 20 mm long. Drop the pitch — M6 × 20 — and the standard coarse pit...Read the full story
14 July 26
The ST L7805CV is the standard three-terminal 5V linear regulator — the TO-220 part that has turned unregulated supplies into clean 5V rails for fifty years. It isn't going anywhere: the 7805 remain...Read the full story
14 July 26
Resistor colour bands encode the value directly: the first bands are digits, the next is a multiplier, and the last is the tolerance. Yellow–violet–red–gold reads as 4, 7, ×100 — 4.7 kΩ at ±5%. Ten co...Read the full story
13 July 26
The short answer
A control panel build needs ten categories of product: enclosure, DIN rail, power supply and distribution, control devices, terminal blocks, internal wiring, cable management, ...Read the full story
13 July 26
Reading a vernier caliper takes two steps: read the whole millimetres from the main scale at the vernier's zero mark, then find the one vernier graduation that lines up exactly with a main-scale line ...Read the full story
10 July 26
A circuit symbol is a standardised shorthand for a component. In the UK, schools, exam boards and industry all use the same standard — BS EN 60617, the British version of the international...Read the full story
10 July 26
Rapid Electronics was proud to support the recent Engineering Student Awards Event at Colchester Institute through the donation of Rapid branded multimeters for award-winning students. Combining p...Read the full story
09 July 26
The K-type is the general-purpose workhorse of temperature measurement: a chromel–alumel thermocouple covering roughly −200°C to +1260°C, cheap to make, tough enough for industrial use and supported...Read the full story
09 July 26
The short answer
A terminal block is chosen on five parameters: pitch, current and voltage rating, conductor cross-section, pole count, and connection method. Pitch is the unforgiving one — i...Read the full story
08 July 26
The MPU6050 motion sensor module has been the default six-axis IMU for a decade of Arduino, Raspberry Pi and micro:bit projects — a three-axis gyroscope and three-axis accelerometer on one chip, tal...Read the full story
07 July 26
Ethernet cables are wired to one of two colour standards: T568A or T568B. Both use the same four twisted pairs - orange, green, blue and brown - and differ only in one detail: the orange and green p...Read the full story
07 July 26
The short answer
Choose an enclosure by working from the environment inwards, not from the PCB outwards. Fix the installation environment first — that sets your IP and IK ratings, which set y...Read the full story
06 July 26
Ohm's law states that the current through a conductor is proportional to the voltage across it: V = I × R, where V is voltage in volts, I is current in amps and R is resistance in ohms. Rearrange it...Read the full story
06 July 26
The Texas Instruments NE555P is the standard bipolar 555 timer in a DIP-8 package, probably the most recognisable IC part number in electronics, and still in volume production more than fifty years ...Read the full story
03 July 26
Converting between temperature scales comes down to two formulas: multiply Celsius by 1.8 and add 32 to get Fahrenheit, and add 273.15 to Celsius to get Kelvin. That covers the arithmetic, but in el...Read the full story
03 July 26
Wire gauge conversion trips people up because three sizing systems are in everyday use in UK workshops: AWG (American Wire Gauge) on imported components and US-authored schematics, metric mm² on Europ...Read the full story
18 June 26
Choosing the right Portable Appliance Testing (PAT) equipment is one of those decisions that looks simple on the surface but can quietly cost or save your business thousands of pounds over time....Read the full story
17 June 26
Industrial automation is changing faster than most budgets can keep up with. Businesses need intelligent systems, AI-driven inspection, predictive maintenance, smart factory integ...Read the full story
17 June 26
Choosing the right transformer is often a balance between performance, cost and physical constraints. For engineers designing audio equipment, semiconductor test systems, medical devices or in...Read the full story
12 June 26
Modern electronic systems are becoming faster, more complex and more integrated than ever before. As a result, engineers face a growing range of test and measurement challenges...Read the full story
11 June 26
Choosing the right test and measurement equipment is an important decision, but choosing the right distributor can be just as critical.
Whether ...Read the full story