Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
  • Suggested Queries

Products

Classroom Bundles

View More Info

These VEX IQ Classroom Bundles are designed to support classroom learning by providing enough equipment to support groups of 10, 20 or 30 students working in groups of two.

Each pair will have a VEX IQ Super Kit 70-7891, containing a VEX IQ Brain, Controller, 4 motors, 7 sensors and 850 structural parts as well as all batteries, chargers and download cables. Each kit is supplied in a stackable storage bin for easy storage at the end of each lesson.

Competition

View More Info

Control

View More Info

VEX IQ Robot Brain

VEX IQ has a powerful Robot Brain with 12 ports which can all be used for either sensors or motors. Connect any combination of up to 12 Smart Port devices to the Robot Brain, which can then be controlled by built-in programs or programmed via a computer and compatible software program. In addition to using pre-programmed instructions, VEX IQ robots can be controlled by drivers using the Controller.

Both the Robot Brain and the Joystick have an integrated (although replaceable!) rechargeable battery which is capable of running robots for hours. The Joystick can be recharged by simply plugging into a USB port.

Motion

View More Info

Smart Motors

The Smart Motor does more than just make your wheels spin or arm move. The built in processor, quadrature encoder and current monitor allow for advanced control and feedback through the Robot Brain. This allows you to program the motor to move very precisely, either by an exact number of rotations or number of degrees.

The motors are easily connected to any other structural parts using the same pins.

Power

View More Info

Programming

View More Info

Sensors

View More Info

In order to allow your robot to interact with its environment, the VEX IQ system has a large range of sensors which can plug into any port on the Robot Brain. The table below gives some examples of the many ways in which these sensors can be used

Sensor Function Possible Uses  
Bumper Switch Simple switch detects when it has been pressed
  • Detect collisions with obstacles
  • Use as a limit switch to detect maximum travel of a robot arm
  • Detect when an object has been placed on a platform
VEX IQ Bumper Switch
Colour Sensor Measures the colour and hue of an object
  • Locate an object of a specific colour
  • Select/reject objects on a conveyor system
  • Measure ambient light level
VEX IQ Colour Sensor
Distance Sensor Uses an ultrasonic pulse to determine the distance from an object
  • Detect a collision with an obstacle before it occurs
  • Stop a precise distance from an object
  • Detect the presence of an object on a conveyor system
  • Measure the distance to an object
VEX IQ Distance Sensor
Gyro Sensor Measures rotation and calculates direction
  • Help a robot to travel in a particular direction
  • Use to keep a robot on a particular heading or course
VEX IQ Gyro Sensor
Touch LED Capacitive touch sensor and multicolour LED
  • Detect when a human touches the sensor, but not plastics, metals etc
  • Output and display any colour on the LED
  • Use to signal status or mood
VEX IQ Touch LED

Starter Kits

View More Info

VEX IQ Starter Kits contain everything you need to build working robots, including all necessary batteries and chargers. Available from £324.99.

3 different kits are available:

  • Starter Kit with Sensors- For building autonomous robots
  • Starter Kit with Controller- Use the joystick to control your creation
  • Super Kit- Contains both sensors and a Joystick for the ultimate robot
Order Code Description Robot Brain, Battery & Charger Nº of motors Nº of sensors Nº of structural and motion parts Joystick & Battery Storage bin and Tray Connecting tables
70-7900 Starter Kit w/Controller YES 4 2 650 YES YES YES
70-7901 Starter Kit w/Sensors YES 4 7 650 NO YES YES
70-7902 Super Kit YES 4 7 650 YES YES YES

Here are some of the demo robots that you can build with any of the VEX IQ Starter kits.

Storage

View More Info

Structure

View More Info