It is the detail that sets Schneider apart from other manufacturers – the ‘invisible innovation’ in its switches and push buttons that only engineers and panel builders really get close enough to appreciate. For example, the push buttons that do not rotate in their panels, or the screws that provide an Earthing connection through their panel contacts. Schneider’s market-leading Harmony range of control and signaling components ensure efficient automation, isolation and detection.
The machine control solutions that Schneider develop for industry rely on the strong performance of individual product lines, and the versatility and adaptability of components to work together within the challenges of a real-world environment. Customers also need to keep manufacturing costs low and design time at a premium. Demands for improved safety functionality are growing, and energy efficiency has become a key factor. Innovations reducing the time required for installation and commissioning.
All these factors need to be taken into consideration when integrating control and signaling components into machine, panel and production line builds.