Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
 +44 (0)1206 751166  

Mega Electronics Fine Etch Clear PCB Etchant

<p>An alternative etchant, with superior performace compared to standard ferric chloride.</p>
  • Di-Sodium Peroxodisulphate Hexahydrate
  • Completely odourless
  • Remains clear
  • Does not crystallise out
  • Achieves satisfactory etching in 6 to 8 min. at 45 to 50°C
  • Supplied in packs of approx. 400g or 1.1kg in powder form to produce approx. 2 or 5 litres respectively of working solution
  • 400g pack is supplied as 4x 100g sachets
  • 1.1kg pack is a single large sachet
Suitable for use with etch tanks 34-0760, 34-0764 and 34-0765.
Order codeMftrs Part No.
34-0392600-033400g etchant (2 litres)
34-0394600-0141.1kg etchant (5 litres)


26 May 2015 Question by: Gary
Q. HI, We have used your Ferric Chloride in the past which dissolves nickel as well as the copper .Could you tell me if this product will also dissolve nickel.
A. Hi Gary, thank you for your question. This should not be a problem however you may wish to make a stronger solution, and adjust the temperature and time it is immersed for in the solution.


05 November 2014 Question by: Gary
Q. May be a silly question but is this product compatible with the Mega Electronics Etching Lab station PCB500 I have been previously using ferric chloride pellets in it.
A. Hi Gary. Thank you for your question. This etchant is suitable for use in etching tanks.


20 January 2014 Question by: Richard | Product code: 34-0394
Q. Hi, would this etchant be compatible with the PCB board 34-0176? if not which one would be? thanks.
A. Hi Richard. Thank you for your question. These PCB fine etch crystals would be suitable for use with the mentioned boards.


18 April 2013 Question by: Leanne
Q. Hi how do we dispose of the used etchant?
A. Hi Leanne. Thank you for your question. Once diluted/used this can be taken to the local county council for disposal. If not the copper can be filtered off, and the remaining liquid can be diluted with water to be poured down the drain - however this is not always suitable practice - the remaining copper can then be disposed of in the bin. A waste tip is normally the best option, lots of schools and colleges have a specific collection company that will dispose of old and dangerous chemicals.


06 April 2013 Question by: H KING | Product code: 34-0392
Q. What is chemical name of product for purpose of Workshop shelf labeling
A. Hi H King. Thank you for your question. The active ingredient is disodium peroxodisulphate Hexahydrate.


30 March 2013 Question by: Nick Cutmore
Q. The smaller pack of this etchant is suppied in 4 x 100g pouches, which allows making up only 0.5 litre at a time and keeping the rest of the powder sealed. How is the larger pack shipped ? All in one tin (which might attract damp when opened) or in multiple pouches ike the smaller pack ? Thanks.
A. Hi Nick, thanks for your question. The larger 1.1Kg tub is just a single unit and is not split into smaller items/pouches.


07 May 2012 Question by: Steve Jenkins
Q. What is the shelf life of the working solution once made up.
A. Thanks for your enquiry Steve. Once made up, the shelf life of this product is about 2 months but you can add more etchant to bring it back slightly. Undiluted the crystals can be stored for 2+ years.


03 May 2012 Question by: mark hanson | Product code: 34-0392
Q. 34-0392 will this make 2000ml of pcb etchant solution? Trying to keep my costs down, radio shack do it already bottled but is 3x as expensive as this if it is the same product. Thank you.
A. Thanks for your enquiry Mark. Yes this product will make 2 litres of PCB etchant solution.


17 April 2012 Question by: Ken Duty | Product code: 34-0394
Q. What is the shelf life of the etchant if stored in its original packaging?
A. Hi Ken, thanks for your question. This is advertised as 2 years, but the manufacture states it is fine up to 5 years, and possibly beyond.


20 March 2012 Question by: Susan
Q. For occasional use i.e. in lab or workshop (not commercial production) is it okay to water wash the PCB after etching with the flushed water going to the normal waste water drain? Obviously the remaining solution in the tank (should it need changing) would be collected in a sealed container and disposed of correctly.
A. Hi Susan, thanks for your question. This would be ok to do, just as long as not lots being done. However the machine is only a water feed down the drain.