This site uses cookies to deliver our services and provide a basic level of website functionality. The four different types of cookies are: Strictly Necessary cookies, Functionality cookies, Performance cookies and Advertising cookies. By checking the box and clicking the button below, you are informing Rapid Electronics Ltd that you agree to the use of these cookies as detailed in our Privacy Policy.

Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
+44 (0)1206 751166

Serial OLED Display Kits - PICAXE

<p>A range of OLED displays and associate components that will provide important components in PICAXE systems. OLEDs are state-of-the-art components that are the future of optoelectronic displays. OLEDs typically have a much brighter display, better viewing angle and lower current consumption than conventional LCD displays and are a feature in many modern electronic devices.<br/><br/> <b>Serial OLED Kit 16 x 2 AXE133Y (13-1276)</b><br/> This budget-conscious serial OLED module, available with a 16 x 2 yellow on black alphanumeric display, allows the visual display of user instructions, sensor reading, etc. of <b>PICAXE</b> microcontroller projects. Connection is via a simple 1-wire serial interface. The included PICAXE-18M2 is fitted on to a small serial interface PCB and is pre-programmed with the open source <b>AXE133</b>/<b>AXE134</b> firmware that allows the microcontroller to act as a 'slave' serial driver for the OLED display. This allows the main project to display text on the OLED via simple 'serout' commands.<br/><br/> The control codes that are used in this kit is identical to those used in the <b>AXE033</b> module, enabling the kit to be used as an alternative to the <b>AXE033</b>. The 18M2 microcontroller can also be reprogrammed, e.g. to change the power-up welcome message. The kit is self-assembly and requires some simple soldering.<br/><br/> <b>Serial OLED/LCD Driver Kit AXE132 (13-1270)</b><br/> The <b>AXE132</b> is the same serial interface board that is supplied in the <b>AXE133Y</b> and <b>AXE134Y</b> kits. The heart of the board is the <b>PICAXE-18M2</b> microcontroller which is pre-programmed with the open source <b>AXE133</b> firmware, allowing the module to drive an OLED or LCD display.</p>
  • Industry proven PICAXE family
  • 16 x 2 or 20 x 4 OLED displays with yellow on black text
  • Simple 1-wire serial connection
  • programmable pre-defined messages
  • Kits supplied complete
For kit contents and assembly instructions see relevant datasheets.
Be the first to ask a question