Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
  • Suggested Queries

Rapid adds over 400 new Europa Components lines

Rapid adds over 400 new Europa Components lines
Rapid Electronics is delighted to announce the introduction of more than 430 new control gear lines from Europa Components into the Rapid catalogue and website.

Europa has over 40 years of expertise in supplying a broad range of electrical components. All products are manufactured to the highest standards, certified in strict accordance with today’s safety standards to give a reliable, safe and industry proven range of quality products.

The new lines added to the Rapid Electronics Catalogue include an impressive choice in sizes of IP65 rated Steel Enclosures and Insulated ABS Enclosures catering for a wide variety of applications. There is also a comprehensive selection of TC1-D range contactors up to 80A, Long Life LED Panel Lamps, 2 and 4 pole Modular Contactors, MCBs, RCBOs, Din Rail Terminals and Accessories. The popular range of Europa Boxed Isolator switches has also been considerably extended to offer a wider choice of enclosure types and switch ratings for greater flexibility.

The introduction of these new lines reflects the on-going, successful and long-standing relationship between Rapid Electronics and Europa Components.

www.rapidonline.com/europa



Share |


Post a Comment