Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
  • Suggested Queries

CamCirc connectors take on the elements

CamCirc connectors take on the elements
CamCirc is the interconnect solution from CamdenBoss that can take on the elements and withstand the worst of nature.

‘WEATHER’ your application be military, industrial, Autosport, medical or marine, CamCirc will perform where other products often fail. From the glamour of the broadcasting world, to the tough demands of the agricultural and construction machinery industries, CamdenBoss's CamCirc range keeps you connected against the elements.

  • IP68 sealed using vacuum technology
  • Multiple options in various body size and types, housing contact configurations from 3 to 19 poles
  • Tough high performance interconnection solution; these connectors will not disconnect when the cable is under physical load or stress
  • Colour coded for ease of connection
  • Ideal for harsh environments and 'glove friendly'
  • Compatible with Fischer products
For example, CamCirc provides the degree of assurance demanded by medical professionals with its IP68 rating, preventing fluid ingress and utilising vacuum seals to stop unintended disconnection. CamCirc also holds its own in the harshest military conditions, able to withstand extreme temperatures, shock, vibration and ensures the highest cable retention capabilities.

www.rapidonline.com/brands/camdenboss





Share |


Post a Comment