Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
 +44 (0)1206 751166  

Taiway Miniature Toggle Switches


<p>These miniature <STRONG>toggle switches </STRONG>from <STRONG>Taiway</STRONG> are available in single pole and double pole options.</p>

  • Contact rating - 5A 125VAC, 2A 250VAC
  • 50,000 make and break cycles at full load
  • Solder lug terminations
  • Epoxy terminal seal
  • Silver plated contacts


 
Contact resistance10mΩ max @ 2-4VDC
Insulation resistance1,000 MΩ min
Dielectric strength1,500V RMS @ sea level
Operating temperature–30°C to +85°C
Materials
CaseDiallylphthalate UL94V-0
Toggle handleBrass, chrome plated
BushingBrass, nickel plated
HousingStainless steel
Question by tom
27 August 2013

Q Hi, I'm looking for a SPDT 3A250VAC, 6A125VAC. On-off-on Please could you point me in the right direction. Thanks
A Hi Tom. Thank you for your question. SPDT on-off-on configuration is 75-0212 5A at 250V AC.

Question by Wauters Pierre
14 June 2013

Q On a testbench - Have a unit with 4 CH BTL and wants to switch between 2 front speakers and 2 rear speakers with only 2 speakers So check as well front as back with only 2 speakers What kind of switch do you propose me ?
A Hi Pierre, thanks for your question. We recommend you using 75-0214 with an ON OFF ON configuration.

Question by Mike | Product code: 75-0212
13 April 2012

Q Im looking to install a switch that allows me to operate a light source of 3.5 DCV. Which one should be the best fit for this job? Thanks.
A Hi Mike, thanks for your question. 75-0211 is the part you require: www.rapidonline.com/Electronic-Components/Miniature-Toggle-Swth-Spdt-75-0211/

Question by Ramunas | Product code: 75-0212
17 March 2012

Q Hi, I'm looking for a switch with the following configuration: 100 SP-3 T5 00 B1 M1 P 0 What would be the correct order code for it?
A Hi Ramunas, thanks for your question. Unfortunately we have no exact match on that code, but something like a 75-0092 may be suitable. If you could provide a little more detail for your requirements we can investigate further.

Question by
09 March 2012

Q can i use it for an LED light and how?
A Yes they can be used for an LED light – it should be inserted into the positive line. The action will depend on the model selected.

Question by allan brady | Product code: 75-0212
24 February 2012

Q Hi, does this switch have momentarily ON then return to centre OFF, then momentarily ON the other way and RETURN to centre OFF,that is in the CENTRE position or OFF when not being operated. Regards Allan
A Hi Allan, thanks for your question. These switches are fixed position. However the 2 below will do that: Single pole version 3 connections: Order code 75-0086 = spdt centre off momentary. Double pole version 6 connections: Order code 75-0090 = dpdt centre off momentary.


loading