Home
Stages
Prizes
Register
Marking
PIC Vehicle
Solar Vehicle
Rules and Regulations
Kit Contents
Hints and Tips
Design Materials
FAQ's
2011-12
2010-11
2009-10
2008-09
2007-08
2006-07
Winners
Videos
Videos
Downloads
About Rapid & Toyota
Toyota Hybrid Snergy Drive

The Toyota Hybrid Synergy Drive

Toyota Auris HSD  

The introduction of the Toyota Hybrid Synergy Drive (HSD) is Toyota’s first step in deploying Hybrid Synergy Drive across its full model range by the 2020s.

The Prius was first introduced in Japan in 1997, making it the first mass produced hybrid vehicle and was subsequently introduced worldwide in 2001. In 2010, the launch of Auris Hybrid, built exclusively at Toyota’s Burnaston factory in the UK, marked the introduction of Toyota’s Hybrid Synergy Drive (HSD) technology to one of its mainstream models for the first time.

This hybrid vehicle uses a combination of petrol engine and electric motor drive to produce outstandingly efficient performance, safety and a major reduction of unwanted emissions.

How it works

A power split device sends part of the petrol engine power to the wheels and part to a generator. The electricity from the generator may go directly to the electric motor to help drive the car, or it may be converted into direct current to be stored in the battery.

For initial acceleration and during low speed driving, the Auris Hybrid’s ultra efficient electric motor uses energy from the battery to power the car. When the energy level is low, the Auris Hybrid uses the petrol engine to power the generator, to recharge the battery.

Above mid range speed, the Auris Hybrid uses both its petrol engine and its electric motor in synergy to power the car. The electric motor gets its energy from a generator also driven by the petrol engine.

When braking and decelerating the Auris Hybrid electric motor is used as a generator which converts otherwise unused kinetic energy into electricity, to recharge the battery.

When the driver activates the EV (Electric Vehicle) mode, the Auris Hybrid is powered solely by the electric motor drawing its energy from the battery.

When stationary, the Auris Hybrid petrol engine switches off to conserve fuel. All other systems including the electric air conditioning continue functioning.

The Environment

When it comes to environmental performance, new Auris Hybrid’s achievements are not just about the fuel economy and low emissions.

Toyota’s determination to reduce emissions and promote sustainability prompted it to specifically develop its own recyclable plastic called Toyota Super Olefin Polymer. This is a resin which has better recyclability than any conventional reinforced composite polypropylene.

CO2 emissions are a best-on-the-market 89g/km, a figure unmatched by any other family car. Moreover, when switched to EV (electric vehicle) running, Auris Hybrid gives zero emissions performance for up to 1.2 miles at speeds up to 31 mph. Toyota has made extensive use of high recyclability materials, and huge efforts to reduce the use of any substances of concern in the car’s construction.

When the EV driving mode button is pressed, the car is powered by the electric motor alone, allowing zero-emission performance and ultra low-noise and smooth motoring, as well as obviously saving on petrol costs.

The car’s engine is designed entirely around conserving energy, while ensuring optimum performance. In a conventional car, each time the brakes are applied, kinetic energy is wasted. Not so in the Auris Hybrid – when braking the electric motor operates as a generator, converting the vehicle’s kinetic energy into electricity, which is used to keep the battery charged. In fact the electric motor is self charging, creating energy from the car’s motion, so you never have to plug the car into the mains.

Even the car’s power steering system is designed to conserve energy, kicking in gradually as and when it’s needed.

When its driving duties are done, more than 85% of new Auris Hybrid can be recycled and more than 95% of its materials can be recovered in a process that only accounts for a tiny proportion (approxi - mately two per cent) of its full lifecycle CO2 emissions.

The Toyota PriusHow it looks

The Auris Hybrid is able to achieve 74.3 miles per gallon on the combined cycle thanks to its low drag coefficient figure.

The Toyota Auris Hybrid is a full hybrid and the undisputed reference point for hybrid technology. It works by using a petrol engine in conjunction with an electric motor which means it can run by using the petrol engine only, electric only or a combination of both. At low speeds or in traffic the Auris Hybrid uses electric power which means zero fuel consumption and zero emissions.

   
Featured Products and Prices are subject to Rapid's standard terms and conditions. Exclusive of VAT at 20%. E&OE
Legal notices | Sitemap