Home
Stages
Prizes
Register
Marking
PIC Vehicle
Solar Vehicle
Rules and Regulations
Kit Contents
Hints and Tips
Design Materials
FAQ's
2011-12
2010-11
2009-10
2008-09
2007-08
2006-07
Winners
Videos
Downloads
About Rapid & Toyota
Toyota Hybrid Synergy Drive

PIC Microcontroller Vehicle

Design Criteria and Vehicle Specifications

PIC Microcontroller Vehicle Design Criteria

Design and build a program-controlled environmentally friendly model vehicle of the future, using a PIC microcontroller to provide in-built intelligence so it can automatically avoid obstacles. The vehicle must include recycled or recyclable components within its design. In competition, the race winning vehicle will be judged to be one that scores the most points over the three attempts. This looks more challenging than it actually is.

Design & Technology National curriculum coverage includes:

  • Knowledge and understanding of systems and control: statements 5 (a) (b) (c) (d) (e)
    Summary: Recognise the elements of systems that can be broken down and the importance of feedback; understand basic principles of electrical, electronic control systems including sensors; understand basic mechanical systems and how these can be linked to other control systems.
  • Evaluating process and products: statements 3 (a) (b) (c)
    Summary: Evaluation of ideas and comparison with original intention; testing and evaluation of prototypes; use of criteria for judging wider fitness for purpose.
  • Knowledge and understanding of control systems: statements 5 (a) i; ii; iii.
    In summary – knowledge and understanding of control process, design of systems, the concept of feedback and analysis of system performance.

PIC Microcontroller Vehicle Specifications

  1. Your vehicle must include recycled or recyclable items within its design and the team must be able to demonstrate features which make the vehicle environmentally friendly.
  2. All electrical components must have been supplied by Rapid (www.rapidonline.com).
  3. Your vehicle must use a programmable PICAXE Microcontroller and obstacle detection device(s) to navigate an obstacle course in the fastest time possible.
  4. Each vehicle must have an on/off switch which is accessible from the outside which enables the power to the motor(s) to be cut.
  5. Maximum length (from the furthest point at the rear to the furthest point at the front) must not exceed 300mm.
  6. Maximum width (from the widest point at left to the widest point at right) must not exceed 190mm.
  7. Maximum height (from ground to highest point) must not exceed 150mm. (Please note the track walls are 50mm in height)
  8. Teams may like to use a body shell to improve aerodynamics and aesthetics. This may not exceed the maximum dimensions outlined above.
  9. All vehicles must have at least three wheels which touch the ground at all times.
  10. You must demonstrate that your vehicle uses an environmental power source. Solar cells do not have to be used in the PIC Microcontroller class, although teams may like to make use of this energy source.

PIC Vehicle IllustrationPIC Microcontroller Vehicle

Resources needed

Control board and motor/gearboxes

Computer for developing control program PICAXE chip, software and download cable.

Vehicles of the future are likely to use electric power, stored in batteries, to propel the vehicle at some point. Therefore, very efficient electric motors and gearboxes are required to get the best performance from these batteries.

It is also likely that vehicles will become more intelligent and will, for instance, be able to avoid obstacles to prevent accidents. Microcontroller chips are already being used in vehicles to provide some intelligence (e.g. automatic windscreen wipers that switch on when it rains) and, in the future, these microcontrollers may also automatically control the steering and braking of the vehicle if a dangerous situation arises.

A microcontroller is often described as a ‘computer-on-a-chip’. It can be used as an electronic brain to control a product, toy or machine. The microcontroller is an integrated circuit (‘chip’) that contains memory (to store the program), a processor (to process and carry out the program) and input/output pins (to connect switches, sensors and output devices like motors).

Microcontrollers are purchased ‘blank’ and then programmed with a specific control program. This program is written on a computer and then ‘downloaded’ into the computer chip. Once programmed, the microcontroller is built into a product to make the product more intelligent and easier to use.

The Toyota Challenge uses a PICAXE microcontroller to control two motors to provide movement and steering for the vehicle. The obstacle detection sensors and control program must be developed by the team entering the competition.

Breaking down the task

The first part of the task is to create a chassis for the vehicle. This can either be designed and built from scratch, or the basic board in the kit can be used. Comprehensive assembly information is provided separately in the control board instructions. The board is fairly easy to construct but should be attempted only by pupils with good soldering skills.

The second part of the task is to design the vehicle, incorporating the control board and user selected sensors/ additional output devices. The microcontroller on the control board provides 5 inputs and 8 outputs. Four outputs (4-7) are pre-configured to drive the motors; all other inputs and outputs are available for the students to use for their vehicle.

The final part of the task is to develop and test the control program for the PICAXE microcontroller. Sample programs are provided in the separate control board instructions, but students will need to further develop their control program.

Design decision considerations may include:

Obstacle detection
In its simplest form, two micro switches (Rapid 78-2408) may be used as the obstacle detection sensors. Alternatively, a high resolution sonar range finder (Rapid 78-1085) may be used to detect obstacles before the vehicle hits them. The sonar sensor can be accurately configured to detect obstacles from 3cm to 3m away.

Choice of motor/gearbox
The choice of motor and gearbox, and accuracy of construction of gearbox, can greatly affect the efficiency of the vehicle. Two gearboxes (Rapid 37-0310) are provided in the starter pack, but students may also consider using a more efficient gearbox (such as Rapid 70-2220).

Battery source
Students may also choose to use alkaline or rechargeable cells. A maximum of 6V is recommended, but which cell size (AA, C etc.) and how many alkaline (1.5V) or rechargeable cells (1.2V) give the best power/weight performance ratio?

footer-picvehicle

   
Featured Products and Prices are subject to Rapid's standard terms and conditions. Exclusive of VAT at 20%. E&OE
Legal notices | Sitemap