*
Rapid logo Bullet  Home  Bullet  Tape Rules  Bullet  Pliers Safety Tips  Bullet  Knives and Blades Tips  Bullet  Hammers  Bullet  Plane Tips
Bullet  Screwdrivers Bullet  Chisels Safety Tips Bullet  Snips 
*
* * *
*
Pliers
*
 Pliers Safety Tips
*
  • Pliers should not be used for cutting hardened wire unless specifically manufactured for this purpose.
  • Never expose pliers to excessive heat. This may draw the temper and ruin the tool.
  • Always cut at right angles. Never rock from side to side or bend the wire back and forth against the cutting edges.
  • Don't bend stiff wire with light pliers. Needle nose pliers can be damaged by using the tips to bend too large a wire. Use a sturdier tool.
  • Never use pliers as a hammer nor hammer on the handles. They may crack or break, or edges may be nicked by such abuse.
  • Never extend the length of handles to secure greater leverage. Use a larger pair of pliers or a bolt cutter.
  • Pliers should not be used on nuts or bolts. A wrench will do the job better and with less risk of damage to the fastener.
  • Oil pliers occasionally. A drop of oil at the hinge will lengthen tool life and assure easy operation.
  • Safety glasses or goggles should be worn when cutting wire, etc. to protect eyes.
*
*
* * *
Terms & Conditions |  Contact