How it works
A power split device sends part of the petrol
engine power to the wheels and part to a
generator. The electricity from the generator
may go directly to the electric motor to help
drive the car, or it may be converted into direct
current to be stored in the battery.
For initial acceleration and during low speed
driving the Prius’ ultra efficient electric motor
uses energy from the battery to power the car.
When the energy level is low, the Prius uses
the electric engine to power the generator, to
recharge the battery.
Above mid range speed, the Prius uses both
its petrol engine and its electric motor in
synergy to power the car. The electric motor
gets its energy from a generator also driven
by the petrol engine. As with low speed
driving, battery recharging may also occur at
the same time.
When braking and decelerating the Prius
electric motor is used as a generator which
converts otherwise unused kinetic energy
into electricity, to recharge the battery.
When the driver activates the EV mode
(Electric Vehicle) mode, the Prius is powered
solely by the electric motor drawing its energy
from the battery.
When stationary, the Prius petrol engine
switches off to conserve fuel. All other
systems including the electric air conditioning
continue functioning.
The Environment
When it comes to environmental performance,
new Prius’s achievements are not
just about the fuel economy and low
emissions. Toyota’s determination to reduce
emissions and promote sustainability
prompted it to research and develop the
world’s first injection moulded material to be
derived from plant matter.
This new Ecological Plastic is used throughout
new Prius. In the short term, Toyota’s aim is
for Ecological Plastic to be used for up to 60
per cent of a car’s interior components.
CO2 emissions are a best-on-the-market
89g/km, a figure unmatched by any other
family car. Moreover, when switched to EV
(electric vehicle) running, Prius gives zero
emissions performance for up to 1.24 miles
at speeds up to 31mph. Inside and out, Toyota
has made extensive use of high-recyclability
materials, and huge efforts to reduce the use
of any substances of concern in the car’s
construction.
When the EV driving mode button is pressed,
the car is powered by the electric motor
alone, allowing zero-emission performance
and ultra low-noise and vibration motoring, as
well as obviously saving on petrol costs.
The car’s engine is designed entirely around
conserving energy, while ensuring optimum
performance. In a conventional car, each time
the brakes are applied, kinetic energy is
wasted. Not so in the Prius – when braking
the electric motor operates as a generator,
converting the vehicle’s kinetic energy into
electricity, which is used to keep the battery
fully charged. In fact the electric motor is selfcharging,
creating energy from the car’s
motion, so you never have to plug the car into
the mains, as with some older fully electric
cars.
Even the car’s power steering system
is designed to conserve energy, kicking in
gradually as and when it’s needed.
When its driving duties are done, more
than 85 per cent of new Prius’s can
be recycled and more than 95 per
cent of its materials can be
recovered in a process that only
accounts for a tiny propor tion
(approximately two per cent) of its
full lifecycle CO2 emissions.
How it looks
The Prius is able to achieve
72.4 miles per gallon on the
combined cycle thanks to its
low drag coefficient figure
placing it as one of the world’s
most aerodynamic vehicles. In
terms of the design, the Prius’
silhouette is iconic – you can spot
a Prius from 100 yards away.
The Toyota Prius is a full hybrid and the
undisputed reference point for hybird
technology. It works by using a petrol engine
in conjunction with an electric motor which
means it can run by using the petrol engine
only, electric only or a combination of both. At
low speeds or in traffic the Prius uses electric
power which means zero fuel consumption
and zero emissions.
Not satisfied with the developments of hybrid
technology, Prius is available with solar
panels fitted on the roof of the car which can
be operated remotely and use fans to cool the
interior of the car without the need to switch
on the engine when parked in open sunshine.
Prius also features a heads up display which
provides vehicle speed and the drivers eco
monitor on the windscreen in the drivers line
of vision meaning eyes do not need to be
taken off the road to check this information. |