Info Zone Info Zone Rapid logo
www.rapidonline.com/infozone
 Infozone > Ecowire

AlphaWireEcoWire™ is a new range of environmentally friendly Hook-Up wire, using a flexible insulation alternative to PVC – Noryl modified polyphenylene ether (mPPE). Inherently lighter, tougher, smaller and more flame resistant than PVC, mPPE is non-halogenic and contains no heavy metal pigments. EcoWire meets RoHS and WEEE requirements for the elimination of hazardous substances and recyclability. Its manufacturers, Alpha Wire, have a 90-year history of industry-leading innovation in cable, wire and tubing products.

Over 50% of the PC manufacturing market have committed to replacing PVC insulated wire with greener alternatives such as EcoWire.

To read on, please select an option from the left hand navigation.

Terms & Conditions |  Website Terms of Use |  Privacy Policy |  Contact |  Sitemap