|
Rapid is committed to supporting the environment, and as part of being a responsible business, sustainability is high on our agenda.
Rapid are proud to be 100% RoHS compliant since 1 July 2006 and WEEE compliant in accordance with EU legislation in 2007. Rapid is a member of WeeCare, and are covered by the WEEE regulations 2006, concerning the disposal of waste electrical and electronic equipment.
Rapid is also a designated collection point in the BatteryBack scheme, which gives customers the facility to dispose of their used or old batteries.
|