*Question functionality currently disabled
05 September 2014 Question by: Rapid Customer
| Product code: 37-2007
Q. is his item something I can print on and personalise using heat press etc
A. Hi Taylor. Thank you for your question. This is just a magnetic sheet, it is not printable itself. The back is sticky so you can stick this sheet to something you have already printed onto card or paper.
03 October 2013 Question by: Rapid Customer
Q. What is the pull force of this material in g/cm²?
A. Hi Tim. Thank you for your question. This is 53 g/cm2.
02 April 2013 Question by: Rapid Customer
Q. is this the material for this sheet electricaly conductive?
A. Hi Chris, thanks for your question. These sheets are not electrically conductive.
30 March 2013 Question by: Rapid Customer
| Product code: 37-2007
Q. Just to clarify - this allows me to attach to plastic (as an example). I would simply peel away the sheet protecting the self adhesive? Once done the card would be able to be stuck to metal?
If I bought the non self adhesive would regular glue allow me to stick it to the plastic? Or would there be a special type of adhesive required?
A. Hi Stuart, thanks for your question. The self-adhesive card will adhere to metal and the non-self adhesive version would stick to plastic using ordinary adhesive.
19 March 2013 Question by: Rapid Customer
Q. Could someone please explain what the difference is between the two A4 0.75mm sheets that you supply? 37-2005 and 37-2007
A. Hi Emma. Thank you for your question. 37-2005 is an A4 magnetic sheet with no adhesive backing whereas 37-2007 is an A4 magnetic sheet with self adhesive backing.