•  Change Product Range 

 +44 (0)1206 751166   Chat to an Online Advisor

Welcome, to enhance your experience we have divided our site into the following sectors. Please choose the one most relevant to you and continue.

We use cookies to ensure that we give you the best experience on our website. If you continue without changing your settings, we'll assume that you are happy to receive all cookies on the Rapid website. However, if you would like to, you can change your cookie settings at any time.

DAS Air Drying Modelling Clay


DAS Air Drying Modelling Clay

DAS
Manufacturer: DAS

 
A fine and even self-hardening modelling clay from DAS.

This air dry clay is one of the many respected products from the range of DAS craft materials. It dries hard to a durable matt finish that can be painted and varnished, and has a multitude of uses both for arts and crafts and around the home.

06-5432 - DAS Air Drying Modelling Clay 500g White
06-5432 - DAS Air Drying Modelling Clay 500g Terracotta
06-5432 - DAS Air Drying Modelling Clay 1kg White
06-5432 - DAS Air Drying Modelling Clay 1kg Terracotta

Das Air Dry Modelling Clay comes sealed in a foil package to keep it fresh and pliable and is available in terracotta or white.





  • No baking required
  • Easy to smooth
  • Can be used with wood, cardboard and terracotta
  • Poster paint and acrylic varnish can be applied for decoration
  • Solid and strong when dry
  • Drying time 24 hours per centimetre thickness
  • PVC free
  • Contains no softeners, only vegetable binders
  • Available in white or terracotta
  • Available in packs of 500g or 1kg


Products
  • DAS Air Drying Modelling Clay 500g White
    DAS Air Drying Modelling Clay 500g White

    (MPN: 3870 00)

    The DAS Air Drying Modelling Clay 500g White is a fine and even self-hardening modelling clay that requires no baking, and can be used with wood, cardboard and terracotta to produce a great range of arts and craft projects, as well as having applications around the home. Rapid...

    Pdf

    Code: 06-5432

    DAS
    1+
    £1.69
    In Stock
    Despatched same day
    DAS Air Drying Modelling Clay 500g Terracotta
    DAS Air Drying Modelling Clay 500g Terracotta

    (MPN: 3871 00)

    The DAS Air Drying Modelling Clay 500g Terracotta is a fine and even self-hardening modelling clay that requires no baking, and can be used with wood, cardboard and terracotta.

    Pdf

    Code: 06-5434

    DAS
    1+
    £1.69
    In Stock
    Despatched same day
    DAS Air Drying Modelling Clay 1kg White
    DAS Air Drying Modelling Clay 1kg White

    (MPN: 3875 00)

    The DAS Air Drying Modelling Clay 1kg White is a fine and even self-hardening modelling clay that requires no baking, and can be used with wood, cardboard and terracotta.

    Pdf

    Code: 06-5436

    DAS
    1+
    £3.19
    In Stock
    Despatched same day
    DAS Air Drying Modelling Clay 1kg Terracotta
    DAS Air Drying Modelling Clay 1kg Terracotta

    (MPN: 3876)

    The DAS Air Drying Modelling Clay 1kg Terracotta is a fine and even self-hardening modelling clay that requires no baking, and can be used with wood, cardboard and terracotta.

    Pdf

    Code: 06-5438

    DAS
    1+
    £3.19
    In Stock
    Despatched same day

Questions


Question by Liz
18 February 2016

QHi please can you tell me what ingredients are in the DAS terracotta modelling clay?
AHi Liz, thank you for your question. The manufacturer states the following: water, inorganic fillers, vegetable bindings.

Question by Matthew
10 February 2016

QHi, I was thinking of using DAS to mould a piece for a small air pipe transition. If it's moulded to about 5mm thickness, when dry would it be able to withstand the pressure of a household vacuum cleaner? Is it possible to mould around an object to prevent internal shrinkage, and if so what be the most suitable material? I was thinking wax might work, as it could be melted later to remove it.
AHi Matthew, thank you for your question. This is not something we have tried, however, we do not see this being a problem and should work. The other option would be something like a silicone sealant, possibly 87-4092.

Question by Veronica
01 February 2016

QHi. Do you know if DAS shrinks once it dries? And if it does, do you know how much is the average shrinkage percent? Thanks.
AHi Veronica, thank you for your question. It would be minimal, approximately 10%.

Question by Terence | Product code: 06-5432
28 January 2016

QHello, is there anything I can add to the white clay to color it while it is wet? I know it comes in different colors but I need to create my own.
AHi Terence, thank you for your question. Possibly a powder paint can be added but would need to be moulded in to change the colour, but it can be painted once dried.

Question by Daniel
29 December 2015

Qonce das is dry is it able to be fibreglassed over? will the resin affect it
AHi Daniel, thank you for your question. As long as the clay has dried completely this should not be an issue.

Question by Serena | Product code: 06-5432
03 December 2015

QHi Can you tell once the clay is dried. Acrylic painted and sealed with varnish is it ok to put in water in a long time?
AHi Serena, thank you for your question. DAS Air Drying Clay is not recommended for use in water.

Question by Sobia | Product code: 06-5432
16 November 2015

QCan you make figures with DAS clay and how do you stop DAS clay from cracking or prevent
AHi Sobia, thank you for your question. You can use this like regular clay. The only difference is that it sets when left in air, no kiln required.

Question by Gemma | Product code: 06-5438
06 November 2015

QHi. How can I make the Clay dry faster??
AHi Gemma, thank you for your question. It is recommended you allow the clay to dry as naturally at room temperature as possible for the best results.

Question by Zahava | Product code: 06-5432
13 July 2015

QCan beads or mosaic tiles be pressed into the wet clay?
AHi Zahava, thank you for your question. We cannot see why this DAS Modelling Clay cannot have beads or mosaic tiles pressed into it.

Question by Matt | Product code: 06-5432
23 June 2015

QI make tiles, can keep it from staying flat, it keep on bending, please advise
AHi Matt, thank you for your question. All we can suggest is placing something heavy on top to keep the tiles flat whilst they set.

Question by mary howard
22 May 2015

Qcan you use a blow dryer to speed up drying time?
AHi Mary, thank you for your question. In theory this may affect the structure of the clay and make it prone to cracking, but as this has not been attempted before you could try drying a small sample first.

Question by andrea
20 March 2015

Qwill DAS hold water once dry?
AHi Andrea, thanks for your question. DAS air drying modelling clay is not suitable for holding water.

Question by Elle
15 December 2014

QOnce fully dried can the made model be vacuum formed?
AHi Elle. Thank you for your question. Once dried it should be strong enough to be used for a template for vacuum forming, however it may depend on small parts as these may be easily damaged.

Question by Kate
24 November 2014

QHi, can I use the air drying clay as a base for mosaic project, once grouted and sealed is it ok to hang it out side?
AHi Kate. Thank you for your question. This is not ideally suited to outdoor use.

Question by Gamel P
24 October 2014

QWhen hardened and fully dry, is the clay frostproof and able to be left outside? Would it need treating with paint or varnish?
AHi Gamel. Thank you for your question. This clay is not waterproof sealing with a varnish will protect it to a point. It is ideally only for indoor use.

Question by Nima
21 August 2014

QHi, what kind of glue can be used to attach dried pieces. I have a project where I made the base and pillars separately, and would like to add the them?
AHi Nima. Thank you for your question. One of the following glues would be suitable: 87-2336 or 87-4044.

Question by Ken Baker
11 August 2014

QWhat is the best way to store any unused clay without it curing
AHi Ken. Thank you for your question. As the clay is dried by air we would suggest you keep any unused clay in an airtight container.

Question by Paul G | Product code: 06-5432
09 June 2014

QHi. Can you tell me the dimensions of the 500g pack of modelling clay please?
AHi Paul. Thank you for your question. The dimensions of the pack of modelling clay are approximately 150mm x 75mm x 35mm.

Question by Tori | Product code: 06-5432
24 April 2014

QCan this clay adhere to vinyl?
AHi Tori. Thank you for your question. This air drying modelling clay will need to be glued to the vinyl once it has hardened.

Question by Christine
10 March 2014

QHi, I understand that Das clay takes 24 hrs to cure but how long is it still workable for? Thanks.
AHi Christine. Thank you for your question. This would be workable for a couple of hours, water can be applied to the surface to make pliable again but does take some time to become soft again.

Question by Tim Simmons
03 February 2014

QWould the 24 drying time for a thick model (circa 1 inch) be lessened if put in a warm airing cupboard?
AHi Tim. Thank you for your question. We would presume the drying/hardening time would be quicker if in a heated room.

Question by cat
21 January 2014

QHow long does it take to dry???
AHi Cat. Thank you for your question. Drying time is approximately 24 hours for each one centimetre thickness.

Question by Paul Olliver
21 November 2013

QCould you tell me if DAS Modelling material contains heavy amounts of sulphur ? I am wanting to use it for casting a silicone mould but the silicone I have will not cure on materials containing heavy amounts of sulphur. Thanks, Paul.
AHi Paul. Thank you for your question. According to the manufacturer, this does not contain any sulphur at all.

Question by Ruby
21 November 2013

QCan you mix in pink food gel colouring to change the colour of the white clay?
AHi Ruby. Thank you for your question. We do not recommend the use of any additive in the DAS clay as it may affect the curing process, you can however use acyrlic paint one the object has dried.

Question by Paul
17 September 2013

QHi Can you use this to build up a multi-part model? My son needs to make a 3D plant cell, I'm wondering if I can make the inside & let it dry, then make the next part around the first part so they fit together, and so on until we've got all the parts? Thanks!
AHi Paul. Thank you for your question. As long as the first layer is completely dry, we see no problem in adding extra layers if required.

Question by Lucy
09 September 2013

QHello. Could you please tell me if DAS is suitable for painting with enamel paint such as humbrol? If so does it require a primer first? Thanks
AHi Lucy. Thank you for your question. It can be painted once dried. You may require several coats for a good colour finish, so I would say a primer would be worth adding first for a good colour finish.

Question by Anya
01 July 2013

QHi i just want to ask a question - if i paint a dried charm i made out of DAS modelling clay with acrylic paint, will i be able to varnish it and if yes, what kind of varnish do you recommend for me to use? thank you so much!
AHi Anya. Thank you for your question. Any sort of varnish should be OK - wood or yacht varnish would be the best option for this application.

Question by hi dear
23 April 2013

Qhi,can we add some organic material to add some porus aspect
AHi Hi Dear. Thank you for your question. You could add some organic material to this - it may need pressing in well to make this hold but it would be ok to do.

Question by Naomi
22 April 2013

QHow harmful is it to sand sculptures made with DAS? Do i need to cover my face? thanks
AHi Naomi. Thank you for your question. This can be sanded down quite safely but always worth wearing dust protectors whilst sanding.

Question by Laura
29 April 2013

QHi! I want to use DAS to give like a wall texture to a model for a project. How I can attach this material to the cardboard from the model?
AHi Laura. Thank you for your question. The cardboard would need some kind of backing for the clay to hold to, so either chicken wire or may be pins/pegs sticking out of the cardboard so the clay can key/hold to once dried.

Question by Holly
08 April 2013

QHi, I am sculpting a crucifixion for a university project, and was wondering if I could sculpt the figure, and then attach it to a wooden cross? Would glue be suitable to do this with?
AHi Holly. Thank you for your question. Although not a guarantee we would suggest the strongest PVA glue available, as this will depend on the overall weight of your figure, whether it is painted or varnished and how porous the wood is.

Question by Daniel G.
22 February 2013

QHi, I am wondering what materials can I use to model clay on that won't stick to when dried? I would need the whole sculpture to come off when dried!
AHi Daniel. Thank you for your question. Usually a smooth plastic board is used - but to be certain - a similar product to that in which it is supplied - such as tinfoil should be suitable.

Question by JOEL B.
08 February 2013

QHi, just want to know if you can seal a hardened DAS clay so that it can be water proof and won't break or soften at all... thanks
AHi Joel. Thank you for your question. This is not waterproof. This an alternative to traditional clay. Painting with a varnish will protect it to an extent.

Question by chris
07 February 2013

QHi, can you use acrylic paint? And can you paint it straight after it's dried or would you need to add some kind of base first?
AHi Chris. Thank you for your question. Acrylic paint can be applied straight after drying.

Question by Julie
21 January 2013

QHi Can you tell once the clay is dried. painted over and sealed with varnish is it ok to put outdoors?
AHi Julie. Thank you for your question. Yes this would work depending on the type of varnish. Any good wood varnish intended for exterior use should be fine. A few coats would be recommended for lasting protection.

Question by jacquie
07 January 2013

QI want to make buttons, is thi clay suitabllle as it will need to be water resistant. Thanks
AHi Jacquie. Thank you for your question. You would need to seal it with a few coats of paint to make it weather resistant

Question by Michael Tizzano
03 January 2013

QAs your DAS product is air-drying, is it possible to mold it around a wire armature, as in making a small dancing figure, without cracks resulting from shrinkage as it dries?
AHi Michael. Thank you for your question. This should be fine to do, you may want to glaze it after drying, to stop it cracking but it shouldn’t really crack - the only thing is the constant movement may cause this but have never tried it. I do think it will be fine to be honest.

Question by Stuart
15 November 2012

QCan I add fresh clay to an already dry piece?
AHi Stuart. Thank you for your question. It is possible to add fresh clay to a hardened piece.

Question by Kathy
30 May 2012

QI am not mathemeticaly gifted ... how thick is one 'cm' ?? as referenced for a 25-hour drying period. Please related it to inches. Thank you.
AThanks for your enquiry Kathy. Since 1inch is the equivalent of 2.54cm. It would take approximately 61 hours for a 1 inch thick piece of clay to completely dry.

Question by Niki
12 March 2012

QShall we use water to form the clay?
AHi Niki, water is not needed to form the clay as this air-hardening DAS modelling clay.

Question by Valerie
16 February 2012

QDo you have to wait until the clay is fully dry before painting?
AHi Valerie, yes it is advisable to wait until the clay is fully dry before painting.

Question by Lindsay | Product code: 06-5432
13 February 2012

QCan the White clay be used for making baby hand a foot prints, then be left out over night to dry?
AHi Lindsay, yes it can be used for this purpose, but drying time is 24 hours per cm thickness.

Question by PJD | Product code: 06-5432
02 November 2011

Qcan you increase DAS fluidity by heating or adding water to fill a small intricate mould
AI'm afraid you cannot add water to this product as this is an Air hardening clay which also means you cannot put this into the oven.


v 3.0

loading


X

2